2018-11-20 11:46 PM
Hello,
I have problems with some STM32F746G-DISCO boards on the USB High speed port.
I have built an application which uses the USB-HS in host mode. On one board, it works fine, but on other ones I cannot make it work.
To test the hardware and not my software, I have built an application with STM32CubeMX with
-> a HID device on USB-FS
-> a VCP device on USB-HS
I have added the necessary initialization sequences for the HS port in the code generated by CubeMX (code below).
The result works fine on one board, I see both devices on the PC
But with other boardss, I see only the FS device.
The board which works is dated 1735 and marked JOVE JVE-M2 94V-0 E232940
One board which does not work is dated 1815 and marked SS-3 14V-0 E229342
Are there some design differences which could explain the problem ?
My initialization code
void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(pcdHandle->Instance==USB_OTG_FS)
{
/* USER CODE BEGIN USB_OTG_FS_MspInit 0 */
/* USER CODE END USB_OTG_FS_MspInit 0 */
/**USB_OTG_FS GPIO Configuration
PA12 ------> USB_OTG_FS_DP
PA11 ------> USB_OTG_FS_DM
*/
GPIO_InitStruct.Pin = OTG_FS_P_Pin|OTG_FS_N_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Peripheral clock enable */
__HAL_RCC_USB_OTG_FS_CLK_ENABLE();
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(OTG_FS_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(OTG_FS_IRQn);
/* USER CODE BEGIN USB_OTG_FS_MspInit 1 */
/* USER CODE END USB_OTG_FS_MspInit 1 */
}
if(pcdHandle->Instance==USB_OTG_HS)
{
/* USER CODE BEGIN USB_OTG_HS_MspInit 0 */
/* USER CODE END USB_OTG_HS_MspInit 0 */
/**USB_OTG_HS GPIO Configuration
PB5 ------> USB_OTG_HS_ULPI_D7
PI11 ------> USB_OTG_HS_ULPI_DIR
PH4 ------> USB_OTG_HS_ULPI_NXT
PB13 ------> USB_OTG_HS_ULPI_D6
PB12 ------> USB_OTG_HS_ULPI_D5
PC0 ------> USB_OTG_HS_ULPI_STP
PA5 ------> USB_OTG_HS_ULPI_CK
PB10 ------> USB_OTG_HS_ULPI_D3
PA3 ------> USB_OTG_HS_ULPI_D0
PB1 ------> USB_OTG_HS_ULPI_D2
PB0 ------> USB_OTG_HS_ULPI_D1
PB11 ------> USB_OTG_HS_ULPI_D4
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_13|GPIO_PIN_12|GPIO_PIN_10
|GPIO_PIN_1|GPIO_PIN_0|GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_HS;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_HS;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_HS;
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_HS;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_HS;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Peripheral clock enable */
__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
__HAL_RCC_USB_OTG_HS_ULPI_CLK_ENABLE();
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(OTG_HS_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(OTG_HS_IRQn);
/* USER CODE BEGIN USB_OTG_HS_MspInit 1 */
/* USER CODE END USB_OTG_HS_MspInit 1 */
}
}
USBD_StatusTypeDef USBD_LL_Init(USBD_HandleTypeDef *pdev)
{
/* Init USB Ip. */
if (pdev->id == DEVICE_FS) {
/* Link the driver to the stack. */
hpcd_USB_OTG_FS.pData = pdev;
pdev->pData = &hpcd_USB_OTG_FS;
hpcd_USB_OTG_FS.Instance = USB_OTG_FS;
hpcd_USB_OTG_FS.Init.dev_endpoints = 6;
hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL;
hpcd_USB_OTG_FS.Init.dma_enable = DISABLE;
hpcd_USB_OTG_FS.Init.ep0_mps = DEP0CTL_MPS_64;
hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
hpcd_USB_OTG_FS.Init.Sof_enable = DISABLE;
hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE;
hpcd_USB_OTG_FS.Init.lpm_enable = DISABLE;
hpcd_USB_OTG_FS.Init.vbus_sensing_enable = DISABLE;
hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE;
if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 0, 0x40);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 1, 0x80);
}
if (pdev->id == DEVICE_HS) {
/* Link the driver to the stack. */
hpcd_USB_OTG_HS.pData = pdev;
pdev->pData = &hpcd_USB_OTG_HS;
hpcd_USB_OTG_HS.Instance = USB_OTG_HS;
hpcd_USB_OTG_HS.Init.dev_endpoints = 8;
hpcd_USB_OTG_HS.Init.speed = PCD_SPEED_FULL; // Changing to PCD_SPEED_HUGH does not help
hpcd_USB_OTG_HS.Init.dma_enable = DISABLE;
hpcd_USB_OTG_HS.Init.ep0_mps = DEP0CTL_MPS_64;
hpcd_USB_OTG_HS.Init.phy_itface = USB_OTG_ULPI_PHY;
hpcd_USB_OTG_HS.Init.Sof_enable = DISABLE;
hpcd_USB_OTG_HS.Init.low_power_enable = DISABLE;
hpcd_USB_OTG_HS.Init.lpm_enable = DISABLE;
hpcd_USB_OTG_HS.Init.vbus_sensing_enable = DISABLE;
hpcd_USB_OTG_HS.Init.use_dedicated_ep1 = DISABLE;
hpcd_USB_OTG_HS.Init.use_external_vbus = DISABLE;
if (HAL_PCD_Init(&hpcd_USB_OTG_HS) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x174);
}
return USBD_OK;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.