2018-11-30 12:50 AM
After the firmwared (or power off-on) and after the reset the same program takes a different amount of time in ticks. Find it in my oun code. Then tried to create code in Cube and check it - same thing. Then I checked clocking settings and frequency - it was same and after power off-on and after reset (HSE 8MHz, Sys 216M). Then I checked systic interruption systic (setting for 1ms), and it always was 1ms.
What to do and why it can be?
For example the simplest program:
volatile uint32_t *DWT_CONTROL = (uint32_t *)0xE0001000;
volatile uint32_t *DWT_CYCCNT = (uint32_t *)0xE0001004;
volatile uint32_t *DEMCR = (uint32_t *)0xE000EDFC;
volatile unsigned int *DWT_LAR = (volatile unsigned int *)0xE0001FB0;
uint32_t Mcounter, count;
main()
{
*DWT_LAR = 0xC5ACCE55; // unlock (CM7)
// enable the use DWT
*DEMCR = *DEMCR | 0x01000000;
// Reset cycle counter
*DWT_CYCCNT = 0;
// enable cycle counter
*DWT_CONTROL = *DWT_CONTROL | 1 ;
SystemClock_Config();
while(1)
{
u8 i=0;
Mcounter=*DWT_CYCCNT;
i =1;
count=*DWT_CYCCNT-Mcounter;
float op_time=count/216.0f;// count/F_CPU
SendToUart(count);
}
}
count after power off-on = 0;
count after reset = 34 ticks;
2018-12-02 9:51 PM
Problem is solved, I use Icache and ART
static void SetSysClock(void)
{
uint32_t PLLM = 8<< RCC_PLLCFGR_PLLM_Pos;
uint32_t PLLN = 432 << RCC_PLLCFGR_PLLN_Pos;
uint32_t PLLP = 0 << RCC_PLLCFGR_PLLP_Pos;
uint32_t PLLQ = 9 << RCC_PLLCFGR_PLLQ_Pos;
/* Configure Flash prefetch, Instruction cache, Data cache and wait state */
SCB_EnableICache();
FLASH->ACR |= FLASH_ACR_LATENCY_7WS;
FLASH->ACR |= FLASH_ACR_ARTEN;
/* Select regulator voltage output Scale 1 mode, EnableOverDriveMode */
PWR->CR1 |= (PWR_CR1_VOS_0 | PWR_CR1_VOS_1) | PWR_CR1_ODEN;
/* Enable HSE */
RCC->CR |= ((uint32_t)RCC_CR_HSEON);
/* Wait till HSE is ready */
while((RCC->CR & RCC_CR_HSERDY)!=RCC_CR_HSERDY){}
/*RCC_PLL_ConfigDomain_SYS*/
RCC->PLLCFGR &=~ RCC_PLLCFGR_PLLSRC | RCC_PLLCFGR_PLLM | RCC_PLLCFGR_PLLN | RCC_PLLCFGR_PLLP | RCC_PLLCFGR_PLLQ; //clear mask
RCC->PLLCFGR = RCC_PLLCFGR_PLLSRC_HSE | PLLM | PLLN | PLLP | PLLQ; //set mask
RCC->CR |= RCC_CR_PLLON;
/* Wait till PLL is ready */
while((RCC->CR & RCC_CR_PLLRDY) != RCC_CR_PLLRDY){}
RCC->CFGR &=~ (RCC_CFGR_HPRE | RCC_CFGR_PPRE1 | RCC_CFGR_PPRE2 | RCC_CFGR_SW);
/*RCC_SetAHBPrescaler HCLK = SYSCLK / 1*/
/*RCC_SetAPB1Prescaler PCLK2 = HCLK / 4*/
/*RCC_SetAPB2Prescaler PCLK2 = HCLK / 2*/
/*RCC_SetSysClkSource*/
RCC->CFGR |= (RCC_CFGR_HPRE_DIV1 | RCC_CFGR_PPRE1_DIV4 | RCC_CFGR_PPRE2_DIV2 | RCC_CFGR_SW_PLL);
/* Wait till System clock is ready */
while((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL) {}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.