2016-01-21 10:43 PM
I cant connect my board because of readout protection is activated (Level 1) and I cant set it back to level 0 in Option Bytes menu on ST-Link Utility. How can I disable Readout Protection please explain in an easy way.
thank you2016-01-22 5:50 AM
Did you enable the readout protection? Or are you just having connectivity issues?
Try strapping BOOT[0] to VDDAlternatively you could use the System Loader to walk the part out via the USART, I believe I've covered the technique here before.The easy way is to provide a method in your own code to undo the protection. ie you code a method in and out2016-01-23 12:59 AM
it's automatic level up to 1 and i dont know why.
i tried connect Boot0 to Vdd and Boot1 to GND, USART was connected, and used flash loader demon before but it wasn't work. it cant connect to the board.2016-01-23 9:46 AM
Ok, lets start with the basics. Make sure you are using a good USB cable, and that you have current versions of the drivers, ST-LINK Utilities, and firmware on the ST-LINK
Try connectivity on a different USB port, a different PC, a different cableWhat version of Windows are you using here.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.