2015-11-27 12:26 AM
Hi all,
I have a problem with programing STM32L15V. I am using about 1m long connection to device from ST Link V2. When I am using STM32 ST-LINK Utility (V3.7.0) there is no problem with connection/programing/erase. When I try to use ST-LINK_CLI (V2.3.0) from command line I can not connect to microcontroler. I have need to use CLI as I need to automate process using LabView. Any idea ? Br, Lucas2015-11-30 3:43 AM
Hi Lucas,
“When I try to use ST-LINK_CLI (V2.3.0) from command line I can not connect to microcontroler.�You may ignored some parameters in your connect command, so it uses the default onestry this -c SWD UR-Syrine-2017-10-11 6:56 PM
Hi Lucas,
I working to automated the CLI process using labview also...can you share the labview vi to me?
Best regards,
Shahril
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.