2015-03-13 2:47 AM
Hi
I use a STM32L100C-DISCO kit. I want to use I2S interface. I configure this interface with STM32CubeMX: I enable I2S2 as Half Duplex Master, I choose HSI and internal clocks to have an audio clock of 48kHz. Everything seems OK and I generate a Keil project (for uVision5). In this project, I try to do a polling I2S request, but unfortunately I never get clocks on SCK and WS pins. I look at these pins with an oscilloscope, but they are stucked at GND. I send you my code :/* Includes ------------------------------------------------------------------*/
&sharpinclude ''stm32l1xx_hal.h''
&sharpinclude ''stm32l100c_discovery.c''
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
I2S_HandleTypeDef hi2s2;
?
/* USER CODE BEGIN PV */
?
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2S2_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
uint16_t RxBuffer[1024];
uint16_t Taille = 512;
uint32_t TimeOut = 1000;
/* USER CODE END 0 */
int main(void)
{
?
/* USER CODE BEGIN 1 */
?
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
BSP_LED_Init(LED3);
BSP_LED_Init(LED4);
MX_I2S2_Init();
/* USER CODE BEGIN 2 */
BSP_LED_On(LED4);
HAL_Delay(1000);
BSP_LED_Off(LED4);
if (HAL_I2S_Receive(&hi2s2, (uint16_t *) RxBuffer, Taille, TimeOut) == HAL_TIMEOUT)
{
BSP_LED_On(LED3);
HAL_Delay(1000);
BSP_LED_Off(LED3);
}
/* USER CODE END 2 */
/* USER CODE BEGIN 3 */
/* Infinite loop */
while (1)
{
BSP_LED_On(LED4);
HAL_Delay(500);
BSP_LED_Off(LED4);
HAL_Delay(500);
}
/* USER CODE END 3 */
}
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLL_DIV3;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
__SYSCFG_CLK_ENABLE();
}
/* I2S2 init function */
void MX_I2S2_Init(void)
{
hi2s2.Instance = SPI2;
hi2s2.Init.Mode = I2S_MODE_MASTER_RX;
hi2s2.Init.Standard = I2S_STANDARD_PHILLIPS;
hi2s2.Init.DataFormat = I2S_DATAFORMAT_24B;
hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;
hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K;
hi2s2.Init.CPOL = I2S_CPOL_LOW;
if (HAL_I2S_Init(&hi2s2) == HAL_OK)
{
BSP_LED_On(LED3);
HAL_Delay(1000);
BSP_LED_Off(LED3);
}
}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__GPIOC_CLK_ENABLE();
__GPIOH_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
/*Configure GPIO pin : PA0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PC8 PC9 */
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_VERY_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
&sharpifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
/* USER CODE END 6 */
}
&sharpendif
Please can you help me? #discovery #i2s2015-03-14 8:51 AM
I don't see any initialization of PB12 and PB13 as Alternate Function 5.
Regards, Hal2015-03-16 7:50 AM
Hal
Thank you for your answer. Initialization of PB12 and PB13 is done in HAL_I2S_MspInit (called by HAL_I2S_Init). Here is the code :void HAL_I2S_MspInit(I2S_HandleTypeDef* hi2s)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hi2s->Instance==SPI2) { /* USER CODE BEGIN SPI2_MspInit 0 *//* USER CODE END SPI2_MspInit 0 */
/* Peripheral clock enable */ __SPI1_CLK_ENABLE(); /**I2S2 GPIO Configuration PB12 ------> I2S2_WS PB13 ------> I2S2_CK PB15 ------> I2S2_SD */ GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_VERY_LOW; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* USER CODE BEGIN SPI2_MspInit 1 */
/* USER CODE END SPI2_MspInit 1 */
}}
I really don't know what's wrong. I changed the speed (from very low to high) but it's not better. Regards, Helene2015-03-19 12:30 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.