2014-08-23 12:13 AM
Hello Sir,
I'm facing the problem with external interrupt while using debugger. I'm using PC14 as external input key and PA15 as normal input key. So,when I was using debugger if I pressed the normal key(PA15) it is activating the external interrupt which is connected to PC14. If I remove the debugger it's working fine. Please Tell me the solution.
#ask-smarter-questions #thanks-and-best-regards2014-08-23 3:50 AM
Very little context to work with here, perhaps you can share some details about the STM32 chip in question, the board, toolchain/debugger, or perhaps some code fragments?
Both pins would share the same EXTI interrupt vector, you'd likely have to filler/qualify the source, and you should be able to differentiate between Line 14 and Line 15. If you poorly construct your IRQHandler it is possible that might re-enter in an undesirable fashion. The use of JTAG might also interfere with the pin use/configuration.2014-08-24 10:35 PM
I'm using STM32F030C6 controller and the debugger is ST-LINK/V2.
Comming to code void EXTI14_Config(void) //PC14 { EXTI_InitTypeDef EXTI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable GPIOA clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); /* Configure PC14 pin as input*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Enable SYSCFG clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Connect EXTI14 Line to PC14 pin */ SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOC, EXTI_PinSource14); //c /* Configure EXTI14 line */ EXTI_InitStructure.EXTI_Line = EXTI_Line14; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable and set EXTI14 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = EXTI4_15_IRQn; //c NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } //Interrupt Handler void EXTI4_15_IRQHandler(void) { if(EXTI_GetITStatus(EXTI_Line14) != RESET) //PC14 { exti_flag = 1; /* Clear the EXTI line 14 pending bit */ EXTI_ClearITPendingBit(EXTI_Line14); } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.