2015-01-12 9:29 AM
Hello, I would like generate two different signal with the channel 1 and 2 of DAC. I've used two different timer (TIM6 and TIM2) and one DMA address (DAC_DHR12RD_Address 0x40007420). I can generate the signals separate but I try to generate the together (each signal with different DAC) It don't work.
Any ideas?? Thank you2015-01-12 9:59 AM
Any ideas??
Like pointing each DMA to the appropriate DAC register?2015-01-12 11:51 PM
This is my code. I generate one signal with DAC1, this is works, but when I try to generate the signal with DAC2 this is works and the signal of DAC1 stops workings
#define DAC_DHR12R1_Adress 0x40007408 #define DAC_DHR12R2_Adress 0x40007414 const uint8_t Escalator8bit[2] = {0x0, 0xFF}; void DMA_Setup(int dec_channel, int8_t DMA_Class, ) { DMA_Channel_TypeDef* DMA_Channel; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; /* DMA operation mode */ DMA_InitStructure.DMA_Priority = DMA_Priority_High; /* Specifies the priority for the DMA Channel */ DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; /* Specifies if the DMAy Channelx will be used in memory-to-memory transfer */ DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; /* Specifies whether the Peripheral address register is incremented or not */ DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; if(dec_channel==0) /* If dec_channel=0 I use DAC1 */ { DMA_InitStructure.DMA_PeripheralBaseAddr = DAC_DHR12R1_Adress; DMA_Channel=DMA2_Channel3; } else { DMA_InitStructure.DMA_PeripheralBaseAddr = DAC_DHR12R2_Adress; DMA_Channel=DMA2_Channel4; } DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&Escalator8bit; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 2; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_DeInit(DMA_Channel); DMA_Init(DMA_Channel, &DMA_InitStructure); /* Enable Channely for DMAx */ DMA_Cmd(DMA_Channel, ENABLE); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.