2010-06-04 10:09 AM
problem with casting between float and int
2011-05-17 4:53 AM
I don't know anything about the
codesourcery compiler but you should not need to cast. The compiler should generate the code to convert int to float without it.
What happens if you remove the cast?
2011-05-17 4:53 AM
the same hardfault exception
2011-05-17 4:53 AM
Do you actually have floating point enabled and properly configured?
Many embedded toolsets default to not providing floating point support because it can be quire resource hungry - see my 1st reply in this thread:[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/usart printf float&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%2520CortexM3%2520STM32/AllItems.aspx¤tviews=231]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fusart%20printf%20float&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FARM%2520CortexM3%2520STM32%2FAllItems%2Easpx¤tviews=2312011-05-17 4:53 AM
What assembly code is the compiler generating for the assignment?
Can you put a breakpoint on this assignment, switch to disassembly mode in the debugger and step through the code instruction by instruction?2011-05-17 4:53 AM
hmm unfortunately I'm new in the arm/cortex world and have prepared by someone a Makefile. As I see there is -mthumb option during compiling and I didn't see any implicite linking oder than library for m3 core... Could you look at this and say where is a mistake?
TOOLCHAIN_BASE = /opt/CodeSourcery/bin/arm-none-eabi-
COMPILE_OPTS = -mcpu=cortex-m3 -mthumb -Wall -g -O0 -mfloat-abi=soft
PROJECT_NAME = plytka
#====================================================
# Paths and directories names
#=====================================================
WORKSPACE_DIR = workspace
PROJECT_DIR = /home/$(USER)/$(WORKSPACE_DIR)/$(PROJECT_NAME)
FIRMWARE_DIR = ./hardware/firmware
SPD_INC_DIR = $(FIRMWARE_DIR)/STM32F10x_StdPeriph_Driver/inc
CMSIS_INC_DIR = $(FIRMWARE_DIR)/CMSIS/Core/CM3
INCLUDE_DIRS = -I. -I$(SPD_INC_DIR) -I$(CMSIS_INC_DIR)
OUTPUT_DIR = $(PROJECT_DIR)/out
DOCS_DIR = $(PROJECT_DIR)/doc
SUBDIRS = hardware
#=====================================================
# Input files
#=====================================================
C_SRC = $(wildcard *.c)
CPP_SRC = $(wildcard *.cpp)
ASM_SRC = $(wildcard *.s)
#===============================================================================
# Output files created from input files
#===============================================================================
CPP_OBJS = $(addprefix $(OUTPUT_DIR)/,$(CPP_SRC:.cpp=.o))
C_OBJS = $(addprefix $(OUTPUT_DIR)/,$(C_SRC:.c=.o))
ASM_OBJS = $(addprefix $(OUTPUT_DIR)/,$(ASM_SRC:.s=.o))
OBJS = $(ASM_OBJS) $(C_OBJS) $(CPP_OBJS) $(USER_OBJS)
#===============================================================================
# tools for compiling, linking and other
#===============================================================================
CC = $(TOOLCHAIN_BASE)gcc
CFLAGS = $(COMPILE_OPTS) $(INCLUDE_DIRS)
CXX = $(TOOLCHAIN_BASE)g++
CXXFLAGS = $(COMPILE_OPTS) $(INCLUDE_DIRS)
AS = $(TOOLCHAIN_BASE)gcc
ASFLAGS = $(COMPILE_OPTS) -c
LD = $(TOOLCHAIN_BASE)gcc
LDFLAGS = -Wl,--gc-sections,-Map=$@.map,-cref,-u,Reset_Handler $(INCLUDE_DIRS) -T $(FIRMWARE_DIR)/stm32.ld
OBJCP = $(TOOLCHAIN_BASE)objcopy
OBJCPFLAGS = -O binary
AR = $(TOOLCHAIN_BASE)ar
ARFLAGS = cr
SIZE = $(TOOLCHAIN_BASE)size
#===============================================================================
# Destination files
#===============================================================================
MAIN_OUT = $(PROJECT_NAME)
MAIN_OUT_ELF = $(MAIN_OUT).elf
MAIN_OUT_BIN = $(MAIN_OUT).bin
#===============================================================================
# main Makefile rule
#===============================================================================
all:
rm -f $(MAIN_OUT_ELF) $(MAIN_OUT_BIN) $(MAIN_OUT_ELF).map
$(shell mkdir $(OUTPUT_DIR) 2>/dev/null)
cd hardware; make all
make this
this: $(OBJS) $(MAIN_OUT_ELF) $(MAIN_OUT_BIN) print_size
#===============================================================================
# compiling - C source -> objects
#===============================================================================
$(OUTPUT_DIR)/%.o : %.c
@echo 'Compiling file: $<'
$(CC) -c $(CFLAGS) $< -o $@
@echo ' '
#===============================================================================
# assembling - ASM source -> objects
#===============================================================================
$(OUTPUT_DIR)/%.o : %.s
@echo 'Assembling file: $<'
$(AS) -c $(ASFLAGS) $< -o $@
@echo ' '
#===============================================================================
# creating destination files
#===============================================================================
$(MAIN_OUT_ELF): $(OBJ)
$(LD) $(LDFLAGS) $(OUTPUT_DIR)/*.o --output $@
$(MAIN_OUT_BIN): $(MAIN_OUT_ELF)
$(OBJCP) $(OBJCPFLAGS) $< $@
2011-05-17 4:53 AM
as I said I can use floating point variables. I.e. function Sin(float) from math.h goes correct and everything its ok.
I disassemble the code and simplifing it looks like:
a = aaa();
val = a+bbb();
=>
8001c40: f7ff ffc4 bl 8001bcc <aaa>
8001c44: 4603 mov r3, r0
8001c46: 607b str r3, [r7, #4]
8001c48: f001 f944 bl 8002ed4 <bbb>
8001c4c: 4603 mov r3, r0
8001c4e: 4618 mov r0, r3
8001c50: f008 ef0a blx 800aa68 <__aeabi_ui2f>
8001c54: 4603 mov r3, r0
8001c56: 4618 mov r0, r3
8001c58: 6879 ldr r1, [r7, #4]
8001c5a: f008 ee28 blx 800a8ac <__addsf3>
....
0800aa68 <__aeabi_ui2f>:
800aa68: e3a03000 mov r3, #0
800aa6c: ea000001 b 800aa78 <__aeabi_i2f+0x8>
'a' is simply just this :
float a = aaa(); // float aaa() {return 2.5;}
and funciton bbb is:
uint32_t bbb();
The exception occurred in the line 8001c5. It didn't jump to <__aeabi_ui2f>...
2011-05-17 4:53 AM
The Cortex-M3 does not support ARM code, only THUMB(2), you are including an ARM library/function and that is why the code traps.
8001c50: f008 ef0a blx 800aa68 <__aeabi_ui2f>
0800aa68 <__aeabi_ui2f>: <= 32 BIT ARM CODE800aa68: e3a03000 mov r3, #0
2011-05-17 4:53 AM
Make sure it is pulling the libraries from a lib/thumb2 directory, I don't use GNU/GCC
2011-05-17 4:53 AM
You CFLAGS contains the correct -mcpu=cortex-m3 -mthumb but the LDFLAGS will also need this info to pull in the correct cortex libs.
Adding COMPILE_OPTS to the LDFLAGS should solve the problem. Cheers sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.