2017-11-12 3:29 PM
Hi.
I configured adc with dma and it doesnt work. I use stm32f030r8t6. When I use only adc and command ADC_GetConversionValue it's all ok.
Here is my code:
/**
****************************************************************************** * @file main.c * @author Ac6 * @version V1.0 * @date 01-December-2013 * @brief Default main function. *******************************************************************************/&sharpinclude 'stm32f0xx.h'&sharpinclude 'stm32f0xx_gpio.h'&sharpinclude 'stm32f0xx_rcc.h'&sharpinclude 'stm32f0xx_adc.h'&sharpinclude 'stm32f0xx_dma.h'&sharpdefine ADC_DR_ADD 0x40;
uint32_t ADC_value;void ADC_init(void)
{ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init(GPIOA,&GPIO_InitStructure); DMA_InitTypeDef DMA_INIT;DMA_INIT.DMA_PeripheralBaseAddr = (uint32_t*) ADC_DR_ADD;
DMA_INIT.DMA_MemoryBaseAddr = (uint32_t)&ADC_value; DMA_INIT.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_INIT.DMA_BufferSize = 1; DMA_INIT.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_INIT.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_INIT.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_INIT.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_INIT.DMA_Mode =DMA_Mode_Circular; DMA_INIT.DMA_Priority = DMA_Priority_High; DMA_INIT.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel1, &DMA_INIT); DMA_Cmd(DMA1_Channel1, ENABLE); ADC_InitTypeDef ADC_INIT;ADC_INIT.ADC_Resolution = ADC_Resolution_10b;
ADC_INIT.ADC_ContinuousConvMode = ENABLE; ADC_INIT.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_INIT.ADC_DataAlign = ADC_DataAlign_Right; ADC_INIT.ADC_ScanDirection = ADC_ScanDirection_Upward; ADC_Init(ADC1, &ADC_INIT);ADC_ChannelConfig(ADC1, ADC_Channel_1 , ADC_SampleTime_55_5Cycles);
ADC_DMACmd(ADC1,ENABLE); ADC_Cmd(ADC1, ENABLE); ADC_GetCalibrationFactor(ADC1); ADC_StartOfConversion(ADC1);}int main(void)
{ADC_init();
while (1) { }}#dma #stm32f0 #adcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.