2017-04-16 4:45 AM
2017-04-18 2:31 AM
Hi,
Do you have SWD mode selected ?
You should configure ST-Link interface as SWD:
Project Options -> ST-LINK -> check SWD Interface option.
Imen
2017-04-18 3:54 AM
I would try a mass-erase, which helps if you have a misbehaving application on the target.
Probably in System Mode (Boot0/Boot1 pins).
2017-04-18 5:36 AM
Hi,
Try to use ST-Link Utility. Then, if still doesn't work, you should check your hardware configuration or check your IAR setting.
Imen
2017-04-19 1:00 AM
Hi Imen
It work fine with ST-Link Uility and function with SWD config in IAR.
Is it(ST-Link V2) SWD interface only?
2017-04-19 1:08 AM
Hi AvaTar
Mass erase has tried but it is still not work(with JTAG config).
Boot0/Boot1 pins are used to select boot location(select bootloader). Right? if not, please correct me.
I guest JTAG & SWD are low level interface to access ARM core no matter what setting of
Boot0/Boot1 pins.
Boot0 =1 & Boot1 =0 : for UART download?
How about another setting? Please share your experience to me.
2017-04-19 2:03 AM
Is it(ST-Link V2) SWD interface only?
For the Discovery and Nucleo boards, yes. Only the stand-alone version supports JTAG.
However, this seems not to be your problem, the error message would look different.
Complains about a non-responsive target means the debug pod is found and is working.
Boot0 =1 & Boot1 =0 : for UART download?
How about another setting? Please share your experience to me.
One of the things I don't memorize - there is an application note from ST, you might try a search.
And, different parts support different interfaces in the system bootloader.
Check the datasheet and/or the reference manual for supported interfaces and the Boot0/Boot1 combinations.
Some boards already have jumpers to support a forced system bootloader entry.
In the long run, I tend to forget those details as well ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.