2017-03-05 10:53 AM
Hi,
I'm working on STM32F091 MCU fora the first time and I'm trying to test the USART1 on PF0,1. I have just wrote the code and it works well, but now I can't receive the RXNE interrupt.. the tx line works normally.. if I try to set the port as an input I see the correct logic level on pin so the port works, it seems that the shift register of USART NOT WORK. Any idea?
Thanks.
lorenzo.
2017-06-15 12:33 PM
You maybe use registry view, which clear status registry flag.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.