2018-01-14 6:14 PM
Greetings everyone,
I have a problem about the output data rate of SDADC1 at STM32F373 MCU.
I use the STM32CubeMX to configure the SDADC1 with single channel, and generate code for Keil uVision 5, I notice that the data output rate is 16.6 kHz under 6 MHz sampling rate,but according to the specification, the data output rate should be 6 MHz/120 = 50 kHz.
If I change to use SDADC2 channel with the same setting, the data output rate can reach 50 kHz correctly, so I think there may be a bug with the HAL driver, did anyone encounter the same problem?
My software version:
STM32CubeMx Version 4.23.0
Keil uVision 5.17.0.0
#stm32f373-sdadcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.