2016-10-30 2:11 AM
Hi All,
I would like to use a queue to send printf outputs to a serial port. When I try to send something into the queue, its freezes after 3rd character. Here is the queue init code:static struct {
osMessageQId receive_queue;
osMessageQId transmit_queue;
}console;
void console_init(void) {
if (!console_stream)
return;
osMessageQDef(transmit_queue,CONSOLE_BUFFER_SIZE, sizeof(uint8_t));
console.transmit_queue = osMessageCreate(osMessageQ(transmit_queue), NULL);
osMessageQDef(receive_queue, CONSOLE_BUFFER_SIZE, sizeof(uint8_t));
console.receive_queue = osMessageCreate(osMessageQ(receive_queue), NULL);
}
here is the putchar code:
PUTCHAR_PROTOTYPE
{
osMessagePut(console.transmit_queue, ch, 100);
return ch;
}
and here is the serial task code:
void console_task_func(void) {
if (!console_stream)
return;
osEvent ev;
for(;;) {
ev = osMessageGet(console.transmit_queue, 100);
if (ev.status==osEventMessage)
HAL_UART_Transmit(console_stream, (uint8_t *)&ev.value, (uint16_t)1, 10U);
}
}
I there any specialities if I want to use it from printf?
thx
Zamek
#queue #printf
2016-11-03 5:34 AM
A couple of things:
You can capture the printf output by implementing ''int _write(int fd, char *ptr, int len)''. Use a mail queue instead of a message queue, it's more efficient. Some example code I use with the STM32F407. printf output is captured an transferred to a diagnostic task using a mail queue. The task transmits the output to a serial port. Not much code, but effective. I'm sure you can improve it. --------------------------------------------------------------------------------/* maximum permissible length of the mail data */
#define DIAG_MAIL_SIZE 255 /* definition of diagnostic serial mail type */ struct DIAG_MAIL { /* an array for holding the data (normally a string) */ char data[DIAG_MAIL_SIZE]; /* the length of the data (normally the length a string) */ uint8_t length; }; --------------------------------------------------------------------------------void MX_FREERTOS_Init(void) {
..... /* USER CODE BEGIN RTOS_QUEUES */ /* DiagSend mail queue */ osMailQDef(DiagSend, 8, struct DIAG_MAIL); DiagSendHandle = osMailCreate(osMailQ(DiagSend), NULL); /* USER CODE END RTOS_QUEUES */ ...... } ---------------------------------------------------------------------------------/* global function to redirect printf */
int _write(int fd, char *ptr, int len) { int result = 0; if ((fd == STDOUT_FILENO) && (ptr != NULL) && (len > 0)) { struct DIAG_MAIL* ptr_mail = osMailAlloc(DiagSendHandle, 0); if (ptr_mail != NULL) { /* if necessary truncate the data length */ if (len > DIAG_MAIL_SIZE) { len = DIAG_MAIL_SIZE; }; /* copy data into the mail message */ arm_copy_q7((q7_t*) ptr, (q7_t*) ptr_mail->data, len); ptr_mail->length = len; /* put the mail into the queue */ osMailPut(DiagSendHandle, ptr_mail); /* return the actual number of bytes placed in mail queue */ result = len; }; }; return result; } ------------------------------------------------------------------------------/* diagnostic serial task function */
void DiagSerTask(void const* argument) { /* task loop */ while (1) { /* wait for an incoming mail */ osEvent evt = osMailGet(DiagSendHandle, osWaitForever); if (evt.status == osEventMail) { /* save pointer to mail */ struct DIAG_MAIL* ptr_mail = evt.value.p; /* transmit over serial port */ HAL_UART_Transmit_IT(&huart2, (uint8_t*) ptr_mail->data, ptr_mail->length); /* wait for notification of transmission completion */ ulTaskNotifyTake(pdTRUE, portMAX_DELAY); /* free mail */ osMailFree(DiagSendHandle, ptr_mail); }; }; } /* serial transmit callback */ void HAL_UART_TxCpltCallback(UART_HandleTypeDef *ptr_huart) { if (ptr_huart->Instance == USART2) { BaseType_t xHigherPriorityTaskWoken = pdFALSE; /* notify task that the serial transmission is completed */ vTaskNotifyGiveFromISR(DiagSerHandle, &xHigherPriorityTaskWoken); /* ensure return to highest priority unblocked */ portYIELD_FROM_ISR(xHigherPriorityTaskWoken); }; } --------------------------------------------------------------------------- stmcube was used to setup USART2. use google to find out more about the printf/_write functions, etc ...2016-11-14 12:25 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.