2024-02-11 4:17 PM
Hello,
After few successful printing using printf and the SWV ITM data console, the console stops showing new data.
To recreate, I created new project, selected the device I have (STM32H723ZGT6), followed the instructions to enable debugging via printf/SWV ITM and run a sample program that just print every 100msec.
As you can see in the screenshot, the prints halt after 360 lines, although the program still runs and I can place an interrupt and see the program and the counter still progress correctly.
Any idea what can cause the printf to stop working?
Thanks!
2024-03-14 8:01 AM
I'm having the same problem with an STM32H745 Discovery board. It will print to the data console for about 15 to 20 seconds and then I have to terminate the debug session and restart it before it will work again. When I step through the _write() function, I see ITM_SendChar() is still being called for each character. I also verified the ITM registers aren't changing (TER, TPR, TCR, LAR, LSR, PID*, CID*) from when it works to when it quits working.
2024-03-15 4:50 PM
@jking Try another host software that displays ITM output. CubeProgrammer, or the CubeIDE debugger with OpenOCD backend ?
2024-03-18 12:58 PM
Thanks for the suggestion, but I gave up on it because it wasn't going to be my long term solution anyway. I assigned the output to a serial port on the dev kit instead of the ITM output and haven't had any problems since.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.