2020-01-06 3:22 PM
I have ST452LE. Code for HAL from Cube MX.
All working fine. The program hex is 50k.
I am just adding another line to main.c
#include "newfile.h" and have the newfile.c int he project.
I am not calling any functions yet into the newfile.c.
Upon flashing all printf's stop working.
41540 1368 6976 49884 c2dc stm452.elf (with the new c file in the folder of the project)
39632 1364 6972 47968 bb60 stm452.elf (without)
```
#include "tca9648.h"
//#include "tla2024.h" //Size : 41008 Bytes WITHOUT
//Size : 42920 Bytes WITH the c file in project
```
I get no errors, or issues compiling, flashing or running, but the __io_putchar wont get called anymore. These printf's are before
starting the rtos kernel right after initializing the UART in the main
function.
LD file:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 160K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 512K
}
RTOS config
#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 7 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)3000)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configUSE_16_BIT_TICKS 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 1
Any idea where to look.
Thank you
2020-01-06 3:43 PM
I found it.
I had 2 functions in the new C files called
uint16_t _write(uint8_t reg_addr)
uint16_t _read(uint8_t reg_addr)
Just renamed them.
// I had this function
uint16_t _write(uint8_t reg_addr)
{
_data.value = 0;
i2c_readbytes(I2C_BUS_NO, _dev_addr, reg_addr, _data.packet, 2);
return _data.value;
}
// weak function overload collision.....
static int _local_write(uint8_t reg_addr)
{
_data.value = 0;
i2c_readbytes(I2C_BUS_NO, _dev_addr, reg_addr, _data.packet, 2);
return _data.value;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.