2024-10-23 5:09 AM
Currently I am Trying to make a custom board for a project now I have done all the decoupling things for the VDD pins however I have to give power supply to the VDDA pin and now I am having some trouble since I am not that expert in hardware. I need few suggestions as for ferrite bead how should I calculate the value needed for that particular board/mcu and I also learned from senior a RLC filter also can do the job perfectly now can someone please suggest me with the guidelines what resources could I follow to learn this things so that I can developed stm32 based board by my self specially this ADC power supply filtering part. I am currently working with STM32F411CEU6
Thanks in Advance.
2024-10-27 8:08 PM
2024-10-27 8:11 PM - edited 2024-10-27 8:12 PM
What could be the general noise source the MCU or the LDO? Additionally, where can I learn about it or check it which components are making noises. I know that LDO have some ripples and we have to take care of that and what else I have to consider
2024-10-27 8:20 PM
Hi,
As I said, mainly the noise is from high frequency part, for example, if there is SDRAM with 100MHz clock on your board, you may pay attention to the 100MHz noise on your board.
Sometime the noise is from the high driver interface, for example, if you run SPI on 20MHz but the signal integrity on the board is not good, the signal will spread its energy, and it would be a noise source.
LDO is a linear part, so it would not spread noise. if there is a DC-DC on the board, we need to take care of its switching frequency as it would be a noise source.
2024-10-28 8:31 AM
Thanks for the answer. I got your point but the main issue is as a under graduation student of Computer Science. I don't have much skills or knowledge in electronics domain. From your answer now I know what to do or what to look after but as I mentioned earlier due to my CS background I don't know how to do those.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.