cancel
Showing results for 
Search instead for 
Did you mean: 

POWER SUPPLY QUERY

seezar
Associate

I am trying to design my own microcontroller and I am following this video  here the guy is using the ams1117 as his linear regulator which has a current output of 1 A, wouldn't this fry the MCU? I read the datasheet for the stm32f405 and in the min/max section it is said that Total current into VDD power lines should be 240mA. I am also looking into using the stm32u5 series the data sheet in that case also says Total current into VDD power lines should be 200mA.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

>>wouldn't this fry the MCU?

That's not how Current works..

 

You have a supply CAPABLE of sourcing 1A, your MCU takes 200 mA in it's usual operations, that means 800 mA is AVAILABLE for other LOAD that presents.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Melc_dB
ST Employee

Hello @seezar,

 

To complete @Tesla DeLorean's response, you can take a look at this wiki page: https://wiki.st.com/stm32mcu/wiki/Basics_of_power_supply_design_for_MCU

It may gives you more informations about designing power supplies.

 

Best regards,

Melchior

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.