2009-01-28 8:58 AM
Power Supply Capacitors
2011-05-17 4:01 AM
I am highly puzzled. Perhaps someone learned can explain this to me.
Figure 11 Power Supply Scheme in the High Density Reference 14611.pdf says an additional 4.7 uF capacitor must be connected to Vdd3. But all power capacitors are connected to the common Vdd source and Vss sink. Should the words actually be ''If Vdd3 is included in the configuration, then an additional 4.7 uF capacitor is required for internal Vdd3 powered circuits.''? Cheers, HalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.