2015-09-10 6:17 AM
Hello,
I use STM32F429I Discovery-Board to make my project and my question is about power supply available on this board.I would to know,if it's possible to recover 3V from P2 if I supply the board by an external dc source with 5v on P1 ?I want to use these 3v to supply an RS232 driver to reach the good logic lvl for USART protocol.thanks.2015-09-10 9:30 AM
There is enough head room in the 3V supply/regulator to use the VDD or 3V on the board to power a MAX3232 chip, or a Bluetooth module, or a GPS receiver. I haven't sat and done the math, but I'd expect you have ~50mA to play with.
If you have higher requirements, the 5V gets you close to 500mA via USB, you can add your own regulators or supplies, common the grounds. If I had a cellular modem wanting 2A peak, I'd use a completely different supply and regulator arrangement. The boards can also be run off those USB Lithium battery pack/chargers (juice boxes, or whatever you want to call them, $20 at WalMart).2015-09-11 5:28 AM
Hi,
thank you for your answer, If I understood it will depend of current's consumption of my elements.Anyway I will use an external power supply which can provide higher than 1 or 2 A except that this power supply provide 5V. I have not made the addition of the current consumed by elements ( µcontroleur, LCD, Max3232,Led etc..) but I am sure that my power supply will be effective.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.