2008-02-20 3:55 AM
Power Stop -- Auto wake up
2011-05-17 3:24 AM
Hi,
When I configure EXT_Line17(RTC_Alarm) to generate an interrupt, and I Set a alarm, the program don't go in interrupt program. I want do an auto wake up. I program the RTC Alarm to wake up the STM32 each second in case of RTC. void RTC_Configuration(void){ PWR_BackupAccessCmd(ENABLE); BKP_DeInit(); RCC_LSEConfig(RCC_LSE_ON); while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET){} RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); RCC_RTCCLKCmd(ENABLE); RTC_WaitForSynchro(); RTC_SetPrescaler(32767); RTC_WaitForLastTask(); RTC_ITConfig(RTC_IT_ALR, ENABLE); RTC_WaitForLastTask(); } In the main program, there is while(1){ RTC_SetAlarm(RTC_GetCounter()+ 1); RTC_WaitForLastTask(); GPIO_SetBits(GPIOC, GPIO_Pin_9); Delay(3000); //delay 3s //PWR_EnterSTOPMode(PWR_Regulator_ON, PWR_STOPEntry_WFI); //SYSCLKConfig_STOP(); GPIO_ResetBits(GPIOC, GPIO_Pin_9); } Normaly, I should have an interrupt in RTC_Alarm , but the interrupt don't occur. After, I want program the rtc alarm in interrupt of rtc alarm: void RTCAlarm_IRQHandler(void){ if(RTC_GetITStatus(RTC_IT_ALR) != RESET){ EXTI_ClearITPendingBit(EXTI_Line17); RTC_WaitForLastTask(); RTC_ClearITPendingBit(RTC_IT_ALR); RTC_WaitForLastTask(); RTC_SetAlarm(RTC_GetCounter()+ 1); System_Process(); PWR_EnterSTOPMode(PWR_Regulator_ON, PWR_STOPEntry_WFI); } } This soluce don't run to! Thanks for your answers2011-05-17 3:24 AM
I have found my error. I forgot a configuration line to delete another line in a exemple copy (EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.