2010-10-16 10:01 AM
Power Over Internet ( POE)
2011-05-17 5:11 AM
Not sure my internet is powered, ethernet perhaps?
Generally you want them to be robust and fault tolerant, TI has a host of solutions. Do you need it to be 802.3af/at compliant, or you just want to push power over the cable. There are solutions which just push DC over the unused pairs, and crude implementations pretty much just use a regulator at the peripheral end. If you are using unshielded cables that might also be a concern if you have appreciable current, or RF leaking out. http://focus.ti.com/analog/docs/gencontent.tsp?familyId=64&genContentId=938 http://www.ti.com/ww/en/analog/poe/index.htm2011-05-17 5:11 AM
@AlexDion - In case you don't get Clive1's hint, the clue is in the name (or, rather, the acronym):
''Power OverI
nternet (PoE
)'' PoE stands for Power over Ethernet - not Internet!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.