2018-03-01 12:08 AM
I need to select CAN 2.0 controller in my application.I would like to get low cost evaluation board for the same.
Please suggest me STM32 CAN2.0 board so that I can learn CAN.
2018-03-01 12:15 AM
board is there but it has LCD.I don't have to use LCD in my app.
2018-03-01 1:52 AM
Hello
akshaybhavsar30
,I recommend you to use the '
' tool , it will help you to find theSTM32 microcontrollers which may answer your request.
Best Regards
Imen
2018-03-01 2:11 AM
I dont have to select controller.Controller that i select may not have evaluation board.rather i would select evaluation board having CAN,I2C,SPI interfcace
2018-03-01 5:55 AM
You don't have to use the LCD unless you need too. The STM32F429I-DISCO is probably a poor choice for other reasons, including the lack of pins in escape other interfaces. The Nucleo-144 boards offer more opportunity to add your own circuitry and interfaces.
ST's EVAL series boards provide CAN interface(s)
This board using the F107 provides for two
https://www.ebay.com/itm/STM32-ARM-Cortex-M3-STM32F107VCT6-Development-Board/172257169142
as does the
2018-03-01 6:24 AM
Does cortex m3 board has debugger on board?
2018-03-01 7:32 AM
Both cited boards have a 20-pin JTAG connector, you'll need to use an external pod, either a stand-alone ST-LINK, or pin wiring to one onboard a DISCO or NUCLEO board.
2018-03-01 7:36 AM
please send me link for ST link debugger
2018-03-01 7:42 AM
Could you try Google?
http://www.st.com/en/development-tools/st-link-v2.html
2018-03-01 10:38 PM
i would prefer to get Nucleo-144 as having debugger on board.I have gone through them.Almost 20 types of nucleo-144 board are available.I need Ethernet connector,USB,I2C,SPI,CAN.I have selected NUCLEO-F446ZE.But datasheet says ethernet connector is available depensing on STM32 support.What does that mean?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.