2020-05-31 6:04 AM
I've managed to get the DFSDM working with a PDM microphone (on a STM32L496 board) - using direct access to registers. But the documentation often made things more difficult than they needed to be. Just a few extra sentences, less ambiguous language and better graphs could have made the whole process a lot easier, for example -
Besides all of the above, I'm looking forward to being able to use the greater variety of PDM microphones, because the I2S microphones I tried all had poor low frequency response for my application.
2020-06-02 7:01 AM
Hello @Community member ,
Thank you for your reports here. We really appreciate your help to improve our documentation.
I raised your feedback internally to the appropriate team for further review. I will keep you informed about the taken actions/explanation if needed.
Best Regards,
Imen
2020-06-02 5:08 PM
Glad to assist. Sometimes as an engineer you have a part in your hand ( a PDM microphone), and you want to get it up and running as fast as you can. For those of us who prefer the simplicity and efficiency of writing direct to registers, even a simple trace of the registers that need to be initialised to get a microphone running would have saved me hours. Anyway, my PDM microphones that supposedly have a flat frequency response down to 28Hz arrived today - let's see how they go.
2020-06-02 10:30 PM
Clear examples and appnotes.
I'm crying for these here for years.
We've got Cubes instead.
JW
2022-02-21 12:30 AM
Hi gregstm , waclawek.jan ,
We produced application note for better explanation of the DFSDM peripheral (AN4990) - there is written in more "easy" or "less technical" style (less "digital signal processing" theory and more "simple" explanation) how sigma delta modulator works, how works the following filter (averaging), comparison with PWM, understanding the "noise shaping" (with comparison with PWM), graph examples of signals in sigma delta modulator, graphs from digital filters outputs (various filter orders explanation practically), ... and something else. There is also attached XLS file with simulation of DFSDM peripheral and there is XLS sheet for DFSDM peripheral configuration according customer needs (to choose appropriate filter parameters with given input and output parameters of application).
Please try to look on this application note - AN4990:
I hope this AN can offer better understanding of DFSDM with less theory.
The description in reference manual is more technical and more strict according "higher level" theory - for more experienced users. We let more space for simple explanation for less experienced users in application note AN4990.
Regards
Igor
2022-02-22 8:25 AM
Hi Igor,
> There is also attached XLS
Where?
[EDIT] This one https://www.st.com/content/ccc/resource/technical/document/technical_article/group0/1b/40/1d/43/1b/8d/47/65/dfsdm_tutorial/files/dfsdm_tutorial.xlsx/jcr:content/translations/en.dfsdm_tutorial.xlsx ? While in pdf the [TUTORIAL] is highlighted, it does not appear to contain a valid link. [/EDIT]
Thanks,
Jan
@Igor Cesko
2022-02-22 10:06 AM
Hi waclawek.jan
Yes - you are right - the link in PDF is broken. We will update PDF with correct link to XLS file:
Regards
Igor
2022-02-22 9:37 PM
Hi Igor,
thanks for the update. Between the reference manual and the application note, the one thing I think would have helped the most is a simple trace/list of values to write to the DFSDM to get it up and running quickly - then I could study (reverse engineer?) the values and make sense of it that way.
Anyway, the DFSDM works great, and with a high quality PDM microphone it is very sensitive (so sensitive in fact, that I might have to build a soundproof container to try and figure out the noise floor).
2022-02-23 12:00 AM
> That one thing I think would have helped the most is a simple trace/list of values to write to the DFSDM
That's exactly what I meant by clear examples.
AN4990 may be a good introductory material, but it should be followed by "executive" ANs ("dozens of AN per peripheral") and accompanying register-based examples. No, Cubes are not a palatable substitute.
But even then, AN4990/xls could/should refer directly to registers and their fields when talking about individual features, as gregstm said above.
JW
2022-02-23 8:37 AM
Hi waclawek.jan
Yes - we offer examples for DFSDM usage based on HAL functions only (but this is no simple direct write to DFSDM registers). The DFSDM acts as ADC - so its functionality is similar: load into DFSDM registers filters parameters, some clock speed and some optional config parameters and start it as ADC. XLS is designed to help with filter values : what to load into DFSDM registers (filter parameters) according user requirements (for beginners with digital filters).
But we have no simple example which manipulates directly with DFSDM registers. So - some "reverse engineering" for HAL DFSDM examples should be done.
Regards
Igor
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.