2014-08-01 11:51 AM
Hi sir/madam
when I am compiling my code for tcp/ip echoserver and echoclient I am getting the errorerror: storage size of 'echoServAddr' isn't known
. I am compiling the code by using CooCox CoIDE Tool. Here is my code &sharpinclude ''stdio.h'' /* for printf() and fprintf() */ &sharpinclude ''sockets.h'' /* for socket(), bind(), and connect() */ &sharpinclude ''inet.h'' /* for sockaddr_in and inet_ntoa() */ &sharpinclude ''stdlib.h'' /* for atoi() */ &sharpinclude ''string.h'' /* for memset() */ &sharpinclude ''unistd.h'' /* for close() */ &sharpinclude <netdb.h> &sharpinclude <sys/types.h> &sharpdefine MAXPENDING 5 /* Maximum outstanding connection requests */ &sharpdefine AF_INET 2 &sharpdefine PF_INET AF_INET &sharpdefine SOCK_STREAM 1 &sharpdefine IPPROTO_TCP 6 void DieWithError(char *errorMessage); /* Error handling function */ void HandleTCPClient(int clntSocket); /* TCP client handling function */ void tcp_echoserver_init(void) { int servSock; /* Socket descriptor for server */ int clntSock; /* Socket descriptor for client */ struct sockaddr_in echoServAddr; /* Local address */ struct sockaddr_in echoClntAddr; /* Client address */ unsigned short echoServPort; /* Server port */ unsigned int clntLen; /* Length of client address data structure */ //if (argc != 2) /* Test for correct number of arguments */ //{ //fprintf(stderr, ''Usage: %s <Server Port>\n'', argv[0]) ; //exit(1); //} //echoServPort = atoi(argv[l]); /* First arg: local port */ /* Create socket for incoming connections */ if ((servSock = socket(PF_INET, SOCK_STREAM, IPPROTO_TCP)) < 0) DieWithError( ''socket () failed'') ; /* Construct local address structure */ memset(&echoServAddr, 0, sizeof(echoServAddr)); /* Zero out structure */ echoServAddr.sin_family = AF_INET; /* Internet address family */ echoServAddr.sin_addr.s_addr = inet_addr(INADDR_ANY); /* Any incoming interface */ echoServAddr.sin_port = htons(echoServPort); /* Local port */ /* Bind to the local address */ if (bind(servSock, (struct sockaddr *)&echoServAddr, sizeof(echoServAddr)) < 0) DieWithError ( ''bind () failed''); /* Mark the socket so it will listen for incoming connections */ if (listen(servSock, MAXPENDING) < 0) DieWithError(''listen() failed'') ; for (;;) /* Run forever */ { /* Set the size of the in-out parameter */ clntLen = sizeof(echoClntAddr); /* Wait for a client to connect */ if ((clntSock = accept(servSock, (struct sockaddr *) &echoClntAddr, &clntLen)) < 0) DieWithError(''accept() failed''); /* clntSock is connected to a client! */ printf(''Handling client %s\n'', inet_ntoa(echoClntAddr.sin_addr)); HandleTCPClient (clntSock) ; } /* NOT REACHED */ } Please help me to resolve the above mentioned error. Thank u Sir/Madam. #incomplete-type2014-08-01 1:38 PM
I am compiling the code by using CooCox CoIDE Tool.
Try their support forum, looks to either be a compiler issue, or some prior line causing a problem, look at the pre-processor output.2014-08-02 2:06 PM
''I am getting the error
error: storage size of 'echoServAddr' isn't known
.''Would've helped if you'd also highlighted where, exactly, in the code you get that.Anyhow, this means that you don't have a proper definition of'echoServAddr'
at the point where you've tried to use it. Without a proper definition, the compiler can't tell what size it is!Try googling ''incomplete type''eg,http://msdn.microsoft.com/en-us/library/200xfxh6.aspx
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.