2017-03-02 9:57 AM
The new format of code generation makes a BUG in the file: bsp_driver_sd.h
The BUG prevent building FAT_FS modules
To solve the issue line 67 should be changed with the following ones:
&sharpifndef BSP_SD_CardInfo
&sharpdefine BSP_SD_CardInfo HAL_SD_CardInfoTypedef &sharpdefine SD_CardInfo HAL_SD_CardInfoTypedef&sharpendif?DETAILS: there was a typo in the first define (capital vs small cap Typedef vs TypeDef)
The second define is the one required by sd_diskio.c
...Middlewares/Third_Party/FatFs/src/drivers/sd_diskio.c:161:3: error: unknown type name 'SD_CardInfo'
SD_CardInfo CardInfo;This is an error in code generation (e.g. cube program) and not the library files and there is no way to rollback after an update (very annoying). Any help in solving this issue faster is appreciated.
C.Alberto Avizzano
#endifSolved! Go to Solution.
2017-04-11 1:56 AM
Hey Richard,
Thank you for your reply. After 2 days, Finally I found the problem. For efficiency reasons, ST deleted the checking SD status after reading/writing data from/to SD by DMA, and leave that to us to implement our own checking code. So in my code, I waited for DMA transfer complete interrupt after read/write by DMA, and it worked!!! Now my code is more efficient while I'm using FreeRTOS and used OS signals to suspend the current task.
After all, I was expecting ST to write at least an example code or something like that (even not efficient) to give us an idea. It was really confusing.
Regards,
Misagh
2017-05-05 2:02 AM
Hello Misagh92,
Could you tell me where you added that code or it will be nice if you can send your code for DMA.This is my email: j
mailto:ohnrray5@gmail.com
For a week I try to run DMA in my SD card and nothing work
:(
Regards,
John
2017-05-05 3:29 AM
mailto:ohnrray5@gmail.com
2017-05-09 8:24 AM
Hello
Avizzano.Carlo_Alber
,Thanks for highlighting this issue and sorry for the inconvenience it causes.
The fix for this issue will be available in CubeMX4.21 that will come very soon.
Please upgrade your CubeMX release as soon as CubeMX4.21 is available.
BR. Eric
2017-11-14 4:23 AM
Hello ST team
I'm working with
I'm writing to you because I'm working on STM32F746ZGTx, but I have found the same BUG problem with the SD card in CubeMx version 4.23.0 library Firmware package STM32F7 v1.8.0.
Before I was working with CubeMX 4.21.0 and Firmware Package 1.7.0 and the problem with the SD card was solved, now I updated with the new version 4.23.0 and seems the .h and .c files have a lot of changes (for instance
stm32f7xx_hal_sd.c
)Please, could you fix the issues?
best
2017-11-14 7:06 AM
Same request in
https://community.st.com/0D50X00009XkX2BSAV
. Please avoid re-opening old threads as issue isn't the same.To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.