2026-03-26 4:45 AM
I'm in need to scan a bunch of contacts in a 4 rows, 8 column diode matrix configuration. PA0-PA7 are the inputs, PB12-PB15 the outputs. What I'm wondering about is the PA0-WKUP special function in contrary to the rest of inputs (PA1-PA7). Do I have to care about this circumstance?
2026-03-26 5:12 AM
If you're not using the Wakeup feature, you can just use it like any other GPIO.
2026-03-27 10:06 AM
Hello @chriskuku ,
When the WKUP pin is not configured for wakeup, it can be used as a GPIO without introducing unwanted behavior.
With best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.