2012-08-07 2:40 PM
Hello
I implementing something like own watchdog, but I can't reset STM32 in SysTick interrupt. It just stop SysTick interrupts but nothing more.I tried to disable interrupts before, but it is same with:__disable_irq ();NVIC_SystemReset ();Is it possible to reset it in some way while I can't do it in main loop?UPDATE: I check that NVIC_SystemReset dont work even in main loop.. Whole STM32 only stop working, but no resetting.Thanks #stm32-watchdog-system-reset2012-08-07 3:01 PM
Would have expected that would have worked, but haven't tried.
What about something like :IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);
IWDG_SetPrescaler(IWDG_Prescaler_4);
IWDG_SetReload(2);
IWDG_ReloadCounter();
IWDG_Enable();
while(1);
2012-08-07 3:03 PM
You don't have something external driving the RESET high?
2012-08-07 3:10 PM
I am afraid, but it does not help - result is same like with NVIC_SystemReset.
I don't have any pin routed to RESET.. I think something is blocking request for resetting. I use 2 timers, 2 usarts, 1 i2c and some gpios. External crystal and nothing special. Systick is configured with SysTick_Config (SystemCoreClock / 10000); Meybe I have to disable all peripherals first.2014-09-24 3:09 AM
Dear all,
Just to give you a feedback because I ran into issues when I tried to make the NVIC_SystemReset work: it did not... I guess I found why and so far I fixed it: On my side, invoking NVIC_SystemReset() did not work properly. So I tried writing the routine in assembly language just like Clive advised us: AREA |.text|, CODE, READONLY THUMB ALIGN SystemReset PROC EXPORT SystemReset [WEAK] ldr r1, =0xE000ED0C ; NVIC Application Interrupt and Controller ldr r0, =0x05FA0004 ; Magic str r0, [r1, #0] ; Reset self b self bx lr ALIGN ENDP END The outcome is that this code works well. So what's the differences between the code of the NVIC_SystemReset: Maybe this: In assembly: - first we write the magic word - secondly we request the reset Meanwhile in the NVIC_SystemReset() function, we try to do both in the same writing operation. So, let's try it: I retouch the NVIC_SystemReset() in the CMSIS file core_cm3.h (for me) like this: /** \brief System Reset The function initiates a system reset request to reset the MCU. */ __STATIC_INLINE void NVIC_SystemReset(void) { /* Ensure all outstanding memory accesses included buffered write are completed before reset */ __DSB(); SCB->AIRCR = ((0x5FA << SCB_AIRCR_VECTKEY_Pos) | /* Magic word */ (SCB->AIRCR & SCB_AIRCR_PRIGROUP_Msk)); /* Keep priority group unchanged */ SCB->AIRCR = SCB_AIRCR_SYSRESETREQ_Msk; /* Request system reset */ __DSB(); while(1); /* wait until reset */ } Now, NVIC_SystemReset() works perfectly... Best regards, Thierry2014-09-24 5:43 AM
While I appreciate people sharing their experience, in particular successes, I would like to go deeper, because I do not understand at all how this solved your problem. The worst being that you may think it is solved whereas there is still a bug hidden.
First, the assembly code writes the magic word and the request in a single operation, which is close to the behaviour of the original NVIC_SystemReset function. Second, your modification of the NVIC_SystemReset function is a bad idea, and won't work on most projects because it will produce two writes to the register, and the second write (with reset request) will be ignored by the processor because it does not contain the magic word. Could you please double check that your modification has the claimed positive effect ? If yes, I would strongly recommend you to clarify the situation (looking at the assembly code generated) because your modification should have lead to the opposite (no more reset).We’re moving the ST Community to a new platform to give you a better and more reliable community experience.