2017-01-31 12:19 PM
The notes in misc.c for NVIC_Init() state that NVIC_Init() should be called first.
The notes for NVIC_PriorityGroupConfig() list 4 priority groups. What are these priority groups and how are they determined?
There are 5 groups of 4 bits so how are they to be packed into a uint32_t?
The function NVIC_Init() is called more than once in our code, I assume one call to NVIC_PriorityGroupConfig() covers all calls to NVIC_Init() and needs to precede all of them.
Thanks,
JH
Solved! Go to Solution.
2017-01-31 12:56 PM
The processor implementation has 4-bits to describe priority and preemption, you get to determine the split of those 4-bits between the two.
If you split as 2 and 2 you'd get 4 priority levels, and 4 premption levels. Premption means it can interrupt during an interrupt, otherwise they take turns via the tail-chaining as ordered by the priority.
Joseph Yiu has some good books on the Cortex parts
2017-01-31 12:34 PM
Read PM0214, ch. 2.3.6 Interrupt priority grouping.
JW
2017-01-31 12:56 PM
The processor implementation has 4-bits to describe priority and preemption, you get to determine the split of those 4-bits between the two.
If you split as 2 and 2 you'd get 4 priority levels, and 4 premption levels. Premption means it can interrupt during an interrupt, otherwise they take turns via the tail-chaining as ordered by the priority.
Joseph Yiu has some good books on the Cortex parts
2017-01-31 2:49 PM
Thanks. I am gonna have to study that a while.
Having to respond via e-mail as my browser won't bring up the forum
sometimes, just spins.
On Tue, Jan 31, 2017 at 3:34 PM, waclawek.jan <
2017-02-02 2:22 PM
I got it, I just need to spend more time reading it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.