2024-04-30 8:30 AM
I am using nucleof439 to work Lwip, however, when I configure the project in stm32cubeide, I generate the code, and comply the project. It is fine, I also can ping the device, however, when I reenter ping command from windows cmd, the device is blocked, anybody know why?
2024-04-30 8:44 AM
@yang hong wrote:when I reenter ping command from windows cmd, the device is blocked
What do you mean by that?
2024-04-30 10:04 AM - edited 2024-04-30 10:04 AM
Hello,
Do you mean that the ping success only once and the second ping has no response?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.