cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo64p Embedded ST-LINK/V2-1 discription

Uwe Bonnes
Chief
Posted on November 09, 2017 at 18:32

Hello,

the nucleo64p biard user manual DocID030544 Rev 2 tells in chapter 9.4 Embedded ST-LINK/V2-1

The following features are no more supported on ST-LINK/V2-1:

· SWIM interface

· Application voltage lower than 3 V (need to add level shifter to support it)

As the board has level shifters, probably the second point does not apply!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.