2014-05-17 2:48 PM
I trying to send continuous serial data at 115200 baud using USART2 which is connected to the ST-LINK portion of the NUCLEO board. ST-LINK implements a VCP which I'm accessing via a terminal on my PC. If I space the characters out (e.g. send 1 every 100 ms) everything works as expected - terminal on PC is updated with the characters as they are received. If I send batches of characters (e.g. send 5 every 100ms), again everything works as expected. However, if I send continuous characters then the VCP stops working (I receive nothing on the terminal), even though I can see the data being sent on the RX pin of CN3 on the NUCLEO board using an oscilloscope. Additionally the ST-LINK commands from the PC no longer work (I can't debug or load code), nor does the USB drive emulation work. It seems that U2 (STM32F103CBT6) that implements the ST-LINK, USB Drive and VCP ''crashes'' when receiving continuous data at 115200 baud on PA3/STLINK_TX.
Has anyone else experience this?Is this a known limitation, and if so what is the maximum continuous character rate that the ST-LINK VCP can handle?Are there any known work arounds?Would it be possible to get updated ST-LINK firmware for the NUCLEO board that addresses this issue?As a side note, once code has been loaded that sends continuously at 115200 baud you can no longer load code on to the NUCLEO board unless you remove SB13, then load code, then reinstall SB13. #nucleo #stm32 #usart2014-05-18 8:52 AM
I've had Nucleo boards sending via the virtual serial, but did not try saturating the connection.
2014-05-19 8:37 AM
Hello,
may you please firstly check if the firmware is up to date (V2J20M4) by running STLink-Upgrade.exe available at . There is a fix in this version that can explain the issue if you are not up to date (see also the release notes). Best regards2014-05-19 1:36 PM
Thanks for your replies.
I am running firmware V2J20M4.I've done a few more experiments:Any other suggestions?
Is this the right forum to engage the maintainers of STLINK firmware?2014-05-19 3:03 PM
Is this the right forum to engage the maintainers of STLINK firmware?
In my experience probably not, this is a user forum.2014-05-20 8:05 AM
Hello,
is it possible to share your .bin file making crash ? Saturation tests at this baudrate did not show such behaviour so far, most probably there is a difference in the context of both situations. Thank you2014-05-20 8:57 AM
Saturation tests at this baud rate did not show such behaviour so far
Seems to work here too (Win7 x64, V2J20S4), 115200 8N1 saturation code in Keil, debugs and permits access, also functions under ST-LINK Utilities. ________________ Attachments : USART2NUCLEO-L152RE-SATURATE.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzuL&d=%2Fa%2F0X0000000bRJ%2FgSCdl903enAYnsH0EUMLQ8hOjkutaBRn.gnpKe70ckE&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.