2024-06-21 2:40 AM - last edited on 2024-06-21 3:16 AM by mƎALLEm
I am use nucleo-h503rb evk board and i am configure fdcan communication. I have mention below my code please see. I have did not comes output on FDCAN communication.
please send me demo code for that
2024-07-05 1:53 AM
Again how did you connect SN65HVD230 RS pin?
According to the sketch you shared I don't see termination resistors of 120ohm on the bus: https://www.buenoptic.net/encyclopedia/item/544-can-termination-resistors-vital-part.html
2024-07-05 2:04 AM
2024-07-05 2:11 AM - edited 2024-07-05 2:11 AM
Ok what about Rs pin of SN65HVD230? is it connected to the ground? if you have schematics of that module please share it otherwise you need to test it with a multimeter: disconnect the power supply and test the continuity.
2024-07-05 2:37 AM
I have check model. Rs connected Gnd with1k pull down register are there.
2024-07-05 2:42 AM
2024-07-05 2:52 AM
could you please connect the RS directly to the GND?
2024-07-05 3:28 AM
I have Rs pin is connected directly GND. but problem has not resolved.
2024-07-05 3:37 AM
It could be a transceiver or module issue. Try another one.
2024-07-05 3:39 AM
But both models are testing Led blinking, Uart transmission is correctly run.
2024-07-05 3:59 AM
I mean the transceiver or its module not the MCU board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.