2019-04-16 6:20 AM
Hello,
I've been trying to determine which Nucleo board will best fit a project on the drawing board. I've been searching to find a table listing all the board models, their CPUs, peripherals, etc. in order to make the decision easier.
Can anyone point me to it, if it exists?
Thanks in advance,
Dave
2019-04-16 9:33 AM
First use STM32 MCU Finder utility to identify which STM32 family looks fine for functionality.
Then select which nucleo type you need based on number of GPIO needed.
Nucleo comes usually with the big memory brother STM32.
Typical package are 32, 64 and 144 pins for Nucleos.
Nucleo 144 sometime comes with Ethernet and USB pre-wired on board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.