2018-06-07 8:49 AM
Hi,
I am using STM32L496 Nucleo-144 connecting SPI1 to external Adafruit MAX31865 PT100 temp sensor using breadboard with Saleae.
For some reason (I have no clue at all), I got nothing from Saleae.
One thing I kinda of curious is the the pinout. From UM1279 User manual, the pinout are
- SPI_SCK PA5
- SPI1_MISO PA6
- SPI1_MOSI PA7
- SPI1_CS PD14
While from Cube the SPI1_NSS is PA4.
I am assuming SPI1_CS and SPI1_NSS are the same (either Chip Select or Slave Select). Just not sure which one should I follow. I did try both, no luck at all.
Why I am not seeing anything from Saleae? I would think should be a very straight forward thing.
Thanks,
Dick
2018-06-07 11:26 AM
Figured out we need to use PA4 for NSS. PA4 ------> SPI1_NSS
And need to change the BaudRatePrescaler to 32.
hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
2018-06-11 11:21 AM
Now the issue become can't get any data using HAL_SPI_TransmitReceive() function. The in_data always 0 while I am able to see the data from analyzer.
Any suggestions?
Thx
2018-06-11 12:37 PM
Got super low visibility into your code/functionality
Perhaps you're not configuring the pin properly? Clocking on the wrong edge?
SPI3?
PD14 should be viable as a GPIO chip select
2018-06-11 12:45 PM
I am using PA4 connecting to slave CS and SPI_NSS_HARD_OUTPUT. That's the
only way to make it working instead of using PD
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
On Mon, Jun 11, 2018 at 10:37 AM, Clive One <st-microelectronics@jiveon.com>
________________ Attachments : image.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxWu&d=%2Fa%2F0X0000000azL%2Fd0v3zzeOZFgetzuDogXJp9wwPzDdOj7cxXw._.tYpc4&asPdf=false2018-06-11 1:20 PM
Not sure of the SPI_NSS_HARD_OUTPUT functionality, STM32 parts don't do that super well.
Doing SPI on L4 using PA5/PA6/PA7 on a couple of other boards without problem, so shouldn't be inherently broken.
2018-06-11 1:37 PM
I think we might see the issue. From the slave chip MAX31865, the CS should
go active low all the time until the transaction completed.
For the HAL_SPI_TransmitReceive() seems the CS go high in the middle of
transaction. Thx
On Mon, Jun 11, 2018 at 11:22 AM, Clive One <st-microelectronics@jiveon.com>
2018-06-11 2:03 PM
When I sending 2 bytes to slave, the CS pin go high in between.
How come it not active low all the time until over? I even manual set the
pin, doesn't seems have any control.
HAL_GPIO_WritePin( GPIOA, GPIO_PIN_4, GPIO_PIN_RESET ); // NSS1 low
HAL_StatusTypeDef status = HAL_SPI_Transmit(m_spi, (uint8_t *)out_data,
len, 10);
while( m_spi->State == HAL_SPI_STATE_BUSY )
; // wait xmission complete
HAL_GPIO_WritePin( GPIOA, GPIO_PIN_4, GPIO_PIN_SET ); // NSS1 high
2018-06-11 2:20 PM
You should be able to control placement manually, not sure what your issue is. Must obviously wait for last bit of last byte to transit the bus first.
2018-06-11 2:21 PM
Don't configure the NSS output as an alternate-function pin (which puts it under control of the SPI module), just make it a simple GPIO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.