2020-11-24 6:04 AM
no description Bit 28 PWREN: Power interface clock enable
stm32f303VCT6
2020-11-24 6:35 AM
As all other bits in that register, this also enables clock to one of the modules - here, PWR, as documented in chapter 7. That's why the bit is called PWREN, as in PWR ENable.
After each device reset, all peripheral clocks are disabled (except for the SRAM and FLITF).
Before using a peripheral user has to enable its clock in the RCC_AHBENR,
RCC_APB2ENR or RCC_APB1ENR register.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.