cancel
Showing results for 
Search instead for 
Did you mean: 

newest cubeMX (4.25.1) can not be install on macOS high sierra(10.13.3)

Rock Deng
Associate III
Posted on May 11, 2018 at 02:48

It seems that newest cubeMX (4.25.1) can not be install on macOS high sierra(10.13.3). Does any old version works? and please fix the issue of 4.25.1.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
john doe
Lead
Posted on May 15, 2018 at 00:30

its quarantined by the operating system because the st developers dont know how to sign their installers.

try this:

sudo xattr -r -d com.apple.quarantine /path/to/the/installer.app

View solution in original post

9 REPLIES 9
Imen.D
ST Employee
Posted on May 11, 2018 at 12:18

Hello

deng.rock

,

Do you mean '

cubeMX (4.1) can not be installed on macOS high sierra(3)

' ?

Best Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Nawres GHARBI
ST Employee
Posted on May 11, 2018 at 14:50

Hi

deng.rock

‌,

I tested the 4.1 install on MAC high sierra 4 and it is working fine.

Could you please launch the install in command line and give me the log

john doe
Lead
Posted on May 15, 2018 at 00:30

its quarantined by the operating system because the st developers dont know how to sign their installers.

try this:

sudo xattr -r -d com.apple.quarantine /path/to/the/installer.app

Posted on May 15, 2018 at 00:29

Sorry for my poor english. I'v already corrected that.

Posted on May 15, 2018 at 00:31

Thank you very much. I will test it again and again.

Posted on May 15, 2018 at 00:47

It replied '

xattr: No such file: /path/to/the/installer.app

'. Should I have to install or configure something before? 
Posted on May 15, 2018 at 03:04

After updated macOS to version 10.13.4, the issue still exists.

When I double clicked SetupSTM32CubeMX-4.25.1 to implement the install process, it pop up a message that shows

SetupSTM32CubeMX-4.25.1� is an application downloaded from the Internet. Are you sure you want to open it? '

and I choose open it, but nothing happened.

It seems like John doe said, the application was 

quarantined by OS. Maybe I should configure something on macOS before installation.

Posted on May 15, 2018 at 15:55

replace /path/to/the/installer.app with the path to the installer.  sorry, i thought that was obvious.

Posted on May 21, 2018 at 06:48

Thank you very much!!! Issue solved.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.