2015-12-19 9:03 PM
Hello,
I need to configure SD card (SDIO-FATFS) access from PC through USB and copy files. Which example of STM32_USB-FS-Device_Lib_V4.0.0 should I follow for STM32L ? Is it the ''Mass_Storage'' example? Should I need to configure anything more for USB connectivity than these lines of code? int main(void) { Set_System(); Set_USBClock(); USB_Interrupts_Config(); USB_Init(); while (bDeviceState != CONFIGURED); ......... } Thank you.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.