2014-02-07 2:15 AM
Dear
I saw STM32F429 discovery board is MF supported. And I looked up the all functions, and it is not include Ethernet. But, only binary image files are offered on the web site. Is there any way of getting porting source? or anyone who tried to solve the problem adding ethernet to discovery32f429
Regards, Jiwon.
2014-02-07 9:50 AM
The real problem here is that SDRAM + LCD + ETHERNET is conflicted at the pin level. This is only going to be resolved with a different board design, with a higher pin count device.
Now you could perhaps attach an SPI ETHERNET board to it, with all the lameness in performance that would introduce.2014-02-10 6:25 AM
I second the release of the source~!
(If ST reads the forums)-MattWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.