2020-01-22 11:12 PM
What i am currently using to achieve my goal.
Few Details :
1: STM32F103C8 Blue Pill
2: CMISS core Library
3:Datasheet, Reference Manual and Programming Manual
I have attached two files. Which give you some idea that how I want to make These 3 functions. I want to understand at Register level.
I want to configure Registers by myself.
Thanks & Regards
@Vivek yadav
2020-01-25 1:59 AM
you have to add TIM1->EGR , which is for update count
and then get value in
TIMx->CNT ,which will increment as per millisecons
2020-01-25 3:23 AM
.
2020-01-28 1:28 AM
I am Trying to generate 1 sec time delay. So i write a code. In which as per my calculation. LED must Toggle at every 1 sec.
Can Any one guide me Where am i wrong ?
// This header file contains memory mapping of all peripherial
#include "stm32f10x.h"
void toggleLED()
{
GPIOC->ODR ^= GPIO_ODR_ODR13;
}
int main()
{
FLASH->ACR |= FLASH_ACR_LATENCY_0;
// by default HSI is selected which is 8 Mhz
RCC->CR |= RCC_CR_HSION;
while(!RCC_CR_HSIRDY);
// HSI divide by 8 i.e frequancy = 8 Mhz/8 = 1 Mhz
RCC->CFGR |= RCC_CFGR_SW_HSI | RCC_CFGR_HPRE_DIV8 | RCC_CFGR_MCO_HSI;
// Port C and Timer 1 is selected
RCC->APB2ENR |= RCC_APB2ENR_IOPCEN | RCC_APB2ENR_TIM1EN;
/* GPIO Block */
// Pin13,10 Mhz, Analog
GPIOC->CRH |= GPIO_CRH_MODE13_0 ;
/* Timer Block */
TIM1->CR1 |= TIM_CR1_ARPE |
TIM_CR1_CMS_0 |
TIM_CR1_DIR |
TIM_CR1_CEN ;
TIM1->EGR |= TIM_EGR_UG;
TIM1->PSC = 0;// count at every 1 pules
TIM1->ARR = 1000 - 1;
// Tout = (ARR+1)*(PSC+1)/Fclk
// Tout = 1000*1/1 Mhz
// Tout = 1/1000 sec == 1 milli Sec
uint16_t cnt =0;
// After configuraing Timer i am expected to toggle the LED at every 1 sec.
while(1)
{
if(TIM1->CNT == 999)
cnt++;
if(cnt == 1000)
{
cnt =0;
toggleLED();
}
}
}
2020-01-28 2:07 AM
I am getting 3 sec delay
2020-01-28 2:30 AM
Try this code
RCC->APB2ENR |= (1<<0); // Enable clock set as per your controller datasheet
TIM1->PSC = 54000; // My timer clock is 54 Mhz : 54 MHZ/ 54000 == 1 ms cnt
TIM1->EGR = TIM_EGR_UG;
TIM1->CR1 = TIM_CR1_CEN;
you will get ms delay .. i have not used TIM1->ARR , here
2020-01-28 4:31 AM
didn't work for me
2020-02-03 3:32 AM
what is the issue coming ?
is that showing differnt value . or counter does not starts at all ?
2020-02-03 5:05 AM
#include "stm32f10x.h"
#define BIT(x) (1<<x)
void init()
{
RCC->CR |= RCC_CR_HSION;//enable HSI 8 MHz RC Oscillator
RCC->CFGR |= RCC_CFGR_PLLSRC_HSI_Div2; // 8/2 = 4 MHz
RCC->CFGR |= RCC_CFGR_PLLMULL9; // 4*9 = 36 Mhz
RCC->CFGR |= RCC_CFGR_SW_PLL; // PLL selected as system clock
while(!RCC_CFGR_SWS_PLL); // Wait for PLL to be ready
RCC->APB2ENR |= (1<<0); // Enable clock set as per your controller datasheet
RCC->APB2ENR |= RCC_APB2ENR_IOPCEN;//Port C enable
RCC->APB2ENR |= RCC_APB2ENR_TIM1EN;//Timer1 Enable
TIM1->PSC = 36000; // My timer clock is 36 Mhz : 36 MHZ/ 36000 == 1 ms cnt
TIM1->EGR = TIM_EGR_UG;
TIM1->CR1 = TIM_CR1_CEN;
}
void configurePins()
{
// Turn on GPIO C
RCC->APB2ENR |= BIT(4);
// Configure PC13 as an output
GPIOC->CRH |= BIT(20);
GPIOC->CRH &= ~(BIT(23) | BIT(22) | BIT(21) );
}
int main()
{
init();
configurePins();
TIM1->ARR = 1001;
uint16_t cnt =0;
while(1)
{
if(TIM1->CNT == 1000 )
{
cnt++;
}
else if(cnt == 1000)
{
GPIOC->ODR ^= BIT(13);
cnt = 0;
}
}//End-while
}*I wrote this code.
2020-02-08 4:23 AM
Milliseconds - if you're beginner, look at what others have done before you. Implement a software system tick counter and make delay function wait on that. https://www.keil.com/pack/doc/CMSIS/Core/html/group__SysTick__gr.html
Microseconds - a sane code rarely needs such a delays. Forget it for now.
Nanoseconds - there doesn't exist such a thing as a precise nanosecond delays based on software. Only hardware can do it and implementation will always be specific to particular use. Therefore forget it at all.
2020-02-08 5:11 AM
Very precise output timings seems now possible with STM32 having HiResolutionTimer. The learning curve might be steep as it's equivalent to a 4GHz timer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.