2018-07-05 10:36 AM
Hello all,
I am urgently looking for a Flash Programming Algorithm for the S25FL256S or S25FL512S Quad SPI Flash Device. This device will be used on a board with an STM32H743i processor. I use Keil as Development Environment and need a Flash Programming Algorithm for the ULINK / ST Link Programming of the system.
Alternatively we could use the MT25QL512ABA Device from Micron.
It seems that there is currently no Flash Algorithm available for Keil.
I tried to find a similar flash programming algorithm which I could use as a base to develop on, but didn't find something up to now.
Has anybody set up a flash programming algorithm for a similar or same device which I can hook to?
Any help very much appreciated!
Gaby
2018-07-05 2:22 PM
I'd be open to reasonable offers for my time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.