2019-01-04 7:26 AM
Hi.
I use the STM32F107 and shall implement the IWDG to supervise my SW.
But my IWDG init-code (stm32_IwdgSetup(..)):
1) stops/halts the MCU in the "IWDG->KR = 0xCCCC" statement below
2) MCU never proceeds/advances from the "IWDG->KR = 0xCCCC" statement
3) MCU restarts (caused by IWDG?)
4) Re-enter and halts/stops at the same "IWDG->KR = 0xCCCC" statement below, and so on …
__inline static void stm32_IwdgSetup (void) {
// Bit 0 LSION: Internal low-speed oscillator enable
// Set and cleared by software.
// 0: Internal RC 40 kHz oscillator OFF
RCC->CSR |= (1<<0); // LSI (internal low speed oscillator) enable, necessary for IWDG
// Bit 1 LSIRDY: Internal low-speed oscillator ready
// Set and cleared by hardware to indicate when the internal RC 40 kHz oscillator is stable.
// After the LSION bit is cleared, LSIRDY goes low after 3 internal RC 40 kHz oscillator clock
// cycles.
// 0: Internal RC 40 kHz oscillator not ready
// 1: Internal RC 40 kHz oscillator ready
while ((RCC->CSR & (1<<1)) == 0); // wait till LSI is ready
/*--------------------------------------------------------
Define IWDG PR and RLR settings
*-------------------------------------------------------*/
IWDG->KR = 0x5555; // enable write to PR, RLR
IWDG->PR = 1;
IWDG->RLR = 400;
IWDG->KR = 0xAAAA; // Reload the watchdog
IWDG->KR = 0xCCCC; // Start the watchdog (CODE WILL NOT PROCEED FROM HERE !?!?!)
} // end of stm32_IwdgSetupWhat have I overseen?
I appreciate comments on this.
BR Terje Bøhler
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.