2013-06-17 1:37 AM
Hello,
I use the STM32F407 and I have to link 3 different slave devices on the same SPI bus (an accelerometer, a touchpad controller and a screen). I have no other solutions. Each device is activated with chip select pin (CS).The problem is, devices have not the same SPI configuration, for example the accelerometer is driven by a clock at high level by default and the touchpad controller is driven by a clock at low level.Does anyone has already used SPI with different configurations ? Can I change the SPI config each time I want to drive a device ?Thanks for your advice !Jean2013-06-18 2:59 AM
It seems complicated to have something working well and fast. I think I need to change one of my device and make it I2C compatible.
I was thinking SPI is a standard protocol and it's easy to link a lot of ICs but it's not !Anyway thanks for your interesting solutions.2013-06-18 4:20 AM
It is hard for others to really estimate all requirements in context - so this is up to you.
You can build a prototype around some core functionality to prove your design, but this costs time, too. Another idea - you could discard the internal DAC and use the GPIO pins for SPI instead. There are plenty of serial DAC circuits around ...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.