2013-09-13 5:04 PM
Hello,
I tried to read two analog inputs from PA3(ADC1_IN3) and PA5(ADC1_IN5). I expected tmpADC[0] has the input data of PA3 and tmpADC[1] has the input data of PA5. However, both tmpADC[0] and tmpADC[1] always have the input data of PA3. I read reference manual multiple times, but I couldn't figure out what is wrong. Please let me know what is problem. I attached my code below(only ADC part). Thanks &sharpinclude <stm32f4xx.h> void ADC_Init(void) { GPIOA->MODER |= (3UL<<6)|(3UL<<10); /*Set PA3 as an analog input, ADC1_IN3, Set PA5 as an analog input ADC1_IN5*/ GPIOA->PUPDR &= ~((3UL<<6)|(3UL<<10)); /*No Pull up and down resistor*/ RCC->APB2ENR =(1<<8); /*ADC1 clk enable*/ ADC1->CR1 = 0; ADC1->CR2 = (1UL<<0)| /*ADC1 power on */ (1UL<<1); /*Continuous conversion*/ ADC1->SMPR1 = 0; ADC1->SMPR2 = 0; ADC1->SQR1 = (1<<20); /* sequence length: two regular conversions*/ ADC1->SQR2 = 0; ADC1->SQR3 = (3UL<<0)|(5UL<<5); /*1st conversion = ADC1_lN3, 2nd conversion = ADC1_IN5*/ ADC->CCR = (1UL<<16); /*fpclk2/4 = 21Mhz */ } short unsigned int get_ADC(void) { ADC1->CR2 |= (1<<30); while(!(ADC1->SR & 0x2)); return ADC1->DR; } int main (void) { tmpADC[0] = get_ADC(); // expecting have data from ADC1_IN3 tmpADC[1] = get_ADC(); //expecting have data from ADC1_IN5 } #stm32f4 #discovery-board #adc-dma2013-10-08 1:35 PM
I've built a 5x version in Keil that seems serviceable, and produces values in the 0-4095 range, not sure what's going on here.
2013-10-08 10:41 PM
Well I tried the code in a new project and it worked flawlessly even though the code running was identical. Very strange. Thank you for your help.
Chris2014-04-17 2:20 PM
What's the cut-off for ''slow speed''?
2014-04-17 2:32 PM
What's the cut-off for ''slow speed''?
SampleTime+12 vs your ability to service the EOC interrupt. I haven't plotted the curve, DMA requires no thought.The total conversion time is calculated as follows:
Tconv = Sampling time + 12 cycles
Example:
With ADCCLK = 30 MHz and sampling time = 3 cycles:
Tconv = 3 + 12 = 15 cycles = 0.5 μs with APB2 at 60 MHz
2015-01-12 8:46 AM
Clive1
I used your first posted program with a little modification to convert the same channel for 8 times, but I find only the first 4 conversions are ''correct'' and the second 4 conversions are ''wrong''. What is wrong in the program? Please help. the converted values are: 0x819, 0x817, 0x818, 0x818, 0x6F8, 0x638, 0x517, 0x464 The values get smaller and smaller.typedef struct {
int chn_nr; //total channels
uint8 chn[TOTAL_CHN];
} ADCDev;
//const ADCDev adc1 = {8, { 4, 4, 4, 4, 4, 4, 4, 4 } };
const ADCDev adc1 = {8, {16, 16, 16, 16, 16, 16, 16, 16} };
void ADC_Configuration(uint16_t *ADCConvertedValues)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
/* Enable peripheral clocks *************************************************/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* DMA2_Stream0 channel0 configuration **************************************/
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)ADCConvertedValues;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = ADC1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; ///
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
/* DMA2_Stream0 enable */
DMA_Cmd(DMA2_Stream0, ENABLE);
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
ADC_TempSensorVrefintCmd(ENABLE);
/* ADC1 Init ****************************************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = adc1.chn_nr;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel configuration ******************************/
//ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 1, ADC_SampleTime_480Cycles); // PA3
//ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 2, ADC_SampleTime_480Cycles); // PA5
for (int i=0;i<sizeof(adc1.chn_nr);i++)
ADC_RegularChannelConfig(ADC1, adc1.chn[i], i+1, ADC_SampleTime_3Cycles);
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 **************************************************************/
ADC_Cmd(ADC1, ENABLE);
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
}
2015-01-12 10:09 AM
DMA_InitStructure.DMA_BufferSize = ADC1; //????
2015-01-12 12:07 PM
2015-01-12 12:17 PM
The question is still the same, why one the first 4 conversions are OK? I even tried to convert 16 times, but it is only the first 4 are reasonable, and the values are getting smaller and smaller after 4 conversion.
I guess you'd have to ponder the ability of the signal source to supply current to charge the capacitor in the sample circuit, and the sample time?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.