2015-01-12 8:35 AM
The problem is
this:
When reading
FSMC
value
always
returns the previous
value
written
in the
FSMC
.And
you need
a color value
of the pixel
SSD1963 ...
Actually,
what's the catch
???
reads
as:
#define LCD_REG (*((volatile unsigned short *) 0x60000000)) #define LCD_RAM (*((volatile unsigned short *) 0x60020000)) //0x2E read_memory_start LCD_Write_Com(0x2E); rtk[0]=LCD_RAM; //All values
rtk []
are the same
, i.e.,that
has been recorded
last time
(LCD_Write_Com (0x2E))
rtk[1]=LCD_RAM; rtk[2]=LCD_RAM; rtk[3]=LCD_RAM;2015-01-12 10:03 AM
Actually,
what's the catch
???
Is there READ pin on the interface, is that correctly wired up and configured? Can you read back any of the control registers?2015-01-12 10:40 AM
Write Registers
work
.initializing
the display
is normal.
graphics primitives
fully working
.just do not
read
...
2015-01-12 11:20 AM
Write Registers
work
.initializing
the display
is normal.
graphics primitives
fully working
.just do not
read
...
That would seem to constrain your task to the hardware, and peripheral configuration related to the read operation. Start your design review there.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.