2013-01-21 5:53 AM
Hi
friends
I use this program to Read ADC1 Value connected to PC2 portof my
''stm32f4discovery'' card
./****************************************************************************************/
void
ADC_setup( void ){
/* Enable ADC clock (This seems to be a duplicate statement) */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
/*********************************************************/
/* Configure ADC Channel 12 pin as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/*** ADC1 regular channel 12 configuration ***/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 1, ADC_SampleTime_3Cycles);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
}
/*Read potentiometer (voltage) value*/
int
POTGetValue( void ){
ADC_SoftwareStartConv(ADC1);
while
(ADC_GetSoftwareStartConvStatus(ADC1));return
ADC_GetConversionValue(ADC1);}
/****************************************************************************************/
int
main( void ){
ADC_setup();
int
val1 = POTGetValue();puts(val1);
}
It works
, Now i want to display many ADC
conversion for example i want to connect
4 signal to 4 port PC0
, P
C
1,
PC2A
ND PC3.
what are the
modifications to do please ?
I found in d
atasheet t
hat PC2 represent
ADC_Channel_12
that's why i use it
And i use in ligne 19 onenumbe
r
of
conversion
Thank you
#stm32f4discovery #adc2013-01-22 8:03 AM
Your C, and basic flow need work.
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADC1ConvertedValue[0];
..
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
..
int main(void)
{
// Don't repeatedly initialize
ADC_setup();
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
while(1)
{
Display (ADC1ConvertedValue[0]);
Display (ADC1ConvertedValue[1]);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.