2021-11-04 8:31 AM
In the firmware package L0 v1.12.0
In the file "Drivers/STM32L0xx_HAL_Driver/Inc/stm32l0xx_hal_cortex.h"
These are the region sizes defined:
#define MPU_REGION_SIZE_32B ((uint8_t)0x04)
#define MPU_REGION_SIZE_64B ((uint8_t)0x05)
#define MPU_REGION_SIZE_128B ((uint8_t)0x06)
#define MPU_REGION_SIZE_256B ((uint8_t)0x07)
#define MPU_REGION_SIZE_512B ((uint8_t)0x08)
#define MPU_REGION_SIZE_1KB ((uint8_t)0x09)
#define MPU_REGION_SIZE_2KB ((uint8_t)0x0A)
#define MPU_REGION_SIZE_4KB ((uint8_t)0x0B)
#define MPU_REGION_SIZE_8KB ((uint8_t)0x0C)
#define MPU_REGION_SIZE_16KB ((uint8_t)0x0D)
#define MPU_REGION_SIZE_32KB ((uint8_t)0x0E)
#define MPU_REGION_SIZE_64KB ((uint8_t)0x0F)
#define MPU_REGION_SIZE_128KB ((uint8_t)0x10)
#define MPU_REGION_SIZE_256KB ((uint8_t)0x11)
#define MPU_REGION_SIZE_512KB ((uint8_t)0x12)
#define MPU_REGION_SIZE_1MB ((uint8_t)0x13)
#define MPU_REGION_SIZE_2MB ((uint8_t)0x14)
#define MPU_REGION_SIZE_4MB ((uint8_t)0x15)
#define MPU_REGION_SIZE_8MB ((uint8_t)0x16)
#define MPU_REGION_SIZE_16MB ((uint8_t)0x17)
#define MPU_REGION_SIZE_32MB ((uint8_t)0x18)
#define MPU_REGION_SIZE_64MB ((uint8_t)0x19)
#define MPU_REGION_SIZE_128MB ((uint8_t)0x1A)
#define MPU_REGION_SIZE_256MB ((uint8_t)0x1B)
#define MPU_REGION_SIZE_512MB ((uint8_t)0x1C)
#define MPU_REGION_SIZE_1GB ((uint8_t)0x1D)
#define MPU_REGION_SIZE_2GB ((uint8_t)0x1E)
#define MPU_REGION_SIZE_4GB ((uint8_t)0x1F)However, both the ARM documentation and the STM32L0 documentation seem to agree that for this core the minimum size is 256B.
So, shouldn't the first 3 #define's be removed?
2021-11-04 8:37 AM
Or just not use functions you know are absent?
2021-11-04 8:48 AM
Of course I can do that. It's just that having invalid options in the library can cause mistakes or the need to double-check the docs, which wastes time.
This file is not generic to all of STM families, it's tailored to L0, so it could be more accurate.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.