2017-02-09 5:42 AM
has anyone tried to play a video file using the new STM32F77x JPEG codec ?
I use an external Video drive processor, so there is 100% of internal processing power available.
I see this in the attached PDF,
' As the JPEG codec is fully implemented in hardware, it delivers one data pixel per cycle without CPU load. '
' Thanks to this flexible feature and its high level of performances, the jpeg codec can be used for M-JPEG video playback'
Is there any sample code for this ?
how about H.264 ? the new Mpeg-4 / AVC
2017-02-10 4:52 AM
Hello
Marsh.Nick
,Maybe this example in the STM32CubeF7 firmware package helps you, which
demonstrates how to use the HW JPEG decoder to decode an MJPEG video file:
STM32Cube_FW_F7_V1.6.0\Projects\STM32F769I_EVAL\Examples\JPEG\JPEG_MJPEG_VideoDecoding
Hope this helps you.
Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.