2018-08-11 8:43 AM
Hello all.
I'm trying to find a CDC same for the NUCLEO-F746ZG board but the latest cube I've downloaded (STM32Cube_FW_F7_V1.12.0) only contains the following:
Could somebody please point me where I could find an example of setting up CDC for the NUCLEO-F746ZG board please?
Thanks
2018-08-13 2:39 AM
Hello,
There is no CDC example for the NUCLEO-F746ZG board available with STM32CubeF7 firmware package. But, there are CDC examples with STM32756G-EVAL and STM32F769I-EVAL. So, you can get inspired from one of these applications to develop your application.
Note that the available HAL examples are listed in this application note AN4731 : "STM32Cube firmware examples" .
With Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.