2010-08-21 6:45 AM
Missing interrupts on DMA
2011-05-17 5:03 AM
Check that the interrupts *don't* share the same Group/SubPriority
Check that the USART doesn't have any errors pending (overrun, parity, framing, etc) Check that all pending interrupts are actually cleared. Evaluate USART and DMA registers in the MIA condition you describe. (Terminal counts, pending status or errors, etc)2011-05-17 5:03 AM
Hi denis,
I believe that you are facing a priority issue and your software is not fast enough to read the received bytes, therefore you may have an over-run condition. However since you are using DMA which is working on back-to-back this operation behavior will not happen since all received bytes should be transferred correctly to your RAM buffer. I would suggest you to refer to our example on web from the StdPeriph_lib STM32F10x_StdPeriph_Lib_V3.3.0\Project\STM32F10x_StdPeriph_Examples\USART\DMA_Interrupt As reference. Hope it helps you. Cheers, STOne-32.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.