2021-07-25 7:05 AM
I'm using the EXTI1 interrupt and defined the EXTI1 handler like this:
void EXTI1_IRQHandler(void)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_1);
if (GPIOA->IDR & 0x0100 {
EXTI->PR = 1;
(void) EXTI->PR;
NVIC_ClearPendingIRQ(EXTI0_IRQn);
NVIC_EnableIRQ(EXTI0_IRQn);
fun1();
} else {
NVIC_DisableIRQ(EXTI0_IRQn);
EXTI->PR = 1;
(void) EXTI->PR; // wait for hardware
NVIC_ClearPendingIRQ(EXTI0_IRQn);
}When I look at the generated list file, I find this assembly code:
000001d4 <EXTI1_IRQHandler>:
while (__HAL_RTC_ALARM_GET_FLAG(hrtc, RTC_FLAG_ALRAWF) == RESET);
1d4: 4bab ldr r3, [pc, #684] ; (484 <_Min_Heap_Size+0x84>)
1d6: 2102 movs r1, #2
if (count-- == 0U)
1d8: 4aab ldr r2, [pc, #684] ; (488 <_Min_Heap_Size+0x88>)
1da: b5f0 push {r4, r5, r6, r7, lr}
1dc: 6159 str r1, [r3, #20]
1de: 6912 ldr r2, [r2, #16]
1e0: 0792 lsls r2, r2, #30
1e2: d525 bpl.n 230 <EXTI1_IRQHandler+0x5c>
hrtc->Instance->ALRMAR = (uint32_t)tmpreg;
1e4: 4aa9 ldr r2, [pc, #676] ; (48c <_Min_Heap_Size+0x8c>)
hrtc->Instance->ALRMASSR = subsecondtmpreg;
1e6: 2040 movs r0, #64 ; 0x40
__HAL_RTC_ALARMA_ENABLE(hrtc);
1e8: 2401 movs r4, #1
1ea: 4ea9 ldr r6, [pc, #676] ; (490 <_Min_Heap_Size+0x90>)
1ec: 2500 movs r5, #0
1ee: 615c str r4, [r3, #20]
__HAL_RTC_ALARM_ENABLE_IT(hrtc,RTC_IT_ALRA);
1f0: 695b ldr r3, [r3, #20]
1f2: f8c2 0180 str.w r0, [r2, #384] ; 0x180
1f6: 6010 str r0, [r2, #0]
1f8: 6932 ldr r2, [r6, #16]
while(Value >= 10)
1fa: 4ba6 ldr r3, [pc, #664] ; (494 <_Min_Heap_Size+0x94>)
1fc: f402 4060 and.w r0, r2, #57344 ; 0xe000
200: 601a str r2, [r3, #0]
202: f5b0 4f80 cmp.w r0, #16384 ; 0x4000
206: 671d str r5, [r3, #112] ; 0x70
208: d025 beq.n 256 <EXTI1_IRQHandler+0x82>
20a: f5b0 5f00 cmp.w r0, #8192 ; 0x2000
20e: d062 beq.n 2d6 <EXTI1_IRQHandler+0x102>
return HAL_ERROR;
210: f5b0 4fc0 cmp.w r0, #24576 ; 0x6000
hsd->State = HAL_SD_STATE_READY;
214: d040 beq.n 298 <EXTI1_IRQHandler+0xc4>
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_FLAGS);
216: f5b0 4f20 cmp.w r0, #40960 ; 0xa000
hsd->ErrorCode |= HAL_SD_ERROR_DATA_CRC_FAIL;
21a: da61 bge.n 2e0 <EXTI1_IRQHandler+0x10c>
21c: f5b0 4f00 cmp.w r0, #32768 ; 0x8000
220: f000 80c5 beq.w 3ae <EXTI1_IRQHandler+0x1da>
hsd->State = HAL_SD_STATE_READY;
224: 4a9c ldr r2, [pc, #624] ; (498 <_Min_Heap_Size+0x98>)
hsd->Context = SD_CONTEXT_NONE;
226: 4b9d ldr r3, [pc, #628] ; (49c <_Min_Heap_Size+0x9c>)
return HAL_ERROR;
228: 6811 ldr r1, [r2, #0]
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_FLAGS);
22a: 400b ands r3, r1
hsd->State = HAL_SD_STATE_READY;
22c: 6013 str r3, [r2, #0]
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_FLAGS);
22e: bdf0 pop {r4, r5, r6, r7, pc}
return HAL_ERROR;
230: 4c99 ldr r4, [pc, #612] ; (498 <_Min_Heap_Size+0x98>)
hsd->ErrorCode |= HAL_SD_ERROR_RX_OVERRUN;
232: 2040 movs r0, #64 ; 0x40
234: 4a99 ldr r2, [pc, #612] ; (49c <_Min_Heap_Size+0x9c>)
236: 6825 ldr r5, [r4, #0]
238: 4994 ldr r1, [pc, #592] ; (48c <_Min_Heap_Size+0x8c>)
hsd->State = HAL_SD_STATE_READY;
23a: 402a ands r2, r5
23c: 6022 str r2, [r4, #0]
hsd->Context = SD_CONTEXT_NONE;
23e: f8c1 0080 str.w r0, [r1, #128] ; 0x80
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_DATA_FLAGS);
242: f3bf 8f4f dsb sy
hsd->State = HAL_SD_STATE_READY;
246: f3bf 8f6f isb sy
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_DATA_FLAGS);
24a: 2201 movs r2, #1
hsd->State = HAL_SD_STATE_READY;
24c: 615a str r2, [r3, #20]
24e: 695b ldr r3, [r3, #20]
return HAL_OK;
250: f8c1 0180 str.w r0, [r1, #384] ; 0x180
254: bdf0 pop {r4, r5, r6, r7, pc}
256: 6858 ldr r0, [r3, #4]
// fun2(!) followsThis isn't my handler at all. Is there some boiler plate coding responsible for the context switch? Looking further, it seems that EXTI2 and EXTI3 handlers don't contain this boiler plate code.
So would the code shown actually be my EXTI1 handler, even though the source lines shown don't match?
Solved! Go to Solution.
2021-07-27 10:10 AM
You know what? When I was looking closely at the generated assembly source, or rather the generated comments, I noticed that the assembly does match my handler, but the C source lines don't!
So this is a bug after all, although not in code generation. Would gcc be the culprit here, or some other tool? Maybe I should switch to CubeIDE, since TrueSTUDIO isn't updated any more.
2021-07-25 7:34 AM
Your EXTI1_IRQHandler function won't compile as written because it has unbalanced parentheses and unbalanced brackets. Are you sure you're looking at the right files and not files in a different project?
2021-07-25 7:40 AM
Sorry, I copied it manually and replaced some defines. The handler is correct and compiles, though.
And yes, I'm looking at the right file, as it changed today just minutes ago.
2021-07-25 9:54 AM
Clean the project, insert a syntax error into your EXTI1_IRQHandler, and try to compile. It should error out. If it does, fix the error and complete compiling. If that doesn't fix it, not sure what else it could be.
> GPIOA->IDR & 0x0100
This is checking against a reserved bit within IDR. Probably not what you want either.
2021-07-26 8:42 AM
Yes, adding a syntax error to the handler will throw an error at exactly that handler, using the Atollic IDE.
Regarding the (potentially wrong) mask, I had substituted a macro here, and chosen a random value. The actual value is 0x2. Sorry to have led you down the wrong trail.
Do you know if all source code lines will be included in the list file as comments? Because I miss quite a few. And while I'm not surprised that the optimization -O2 shuffles code around, the fun2 in above snippet actually denotes the middle of some other inlined function
Also, what does the code do? I'm not using alarms myself, but I do use the SDMMC1 peripheral. To investigate, I searched for the first line, and found a hit in HAL_RTC_SetAlarm_IT, which also seems to contain the rest of the lines. Again, I have no idea why this is invoked here.
2021-07-26 9:28 AM
2021-07-27 10:10 AM
You know what? When I was looking closely at the generated assembly source, or rather the generated comments, I noticed that the assembly does match my handler, but the C source lines don't!
So this is a bug after all, although not in code generation. Would gcc be the culprit here, or some other tool? Maybe I should switch to CubeIDE, since TrueSTUDIO isn't updated any more.
2021-07-31 9:37 AM
Just for the record: Same behavior with gcc from CubeIDE.
2021-07-31 9:55 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.